<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Problems after OTA update</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Problems-after-OTA-update/m-p/763477#M118602</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sascha Seefelder,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The VAR-SOM products are supported by Variscite. If the Android image you downloaded on the board is from Variscite’s BSP and does support OTA updates I would recommend contacting them or looking at their forums.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Another alternative would be considering Android-centric forums such as Google’s developer’s portal, as this function changes significantly between Android revisions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Nov 2017 21:13:29 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2017-11-15T21:13:29Z</dc:date>
    <item>
      <title>Problems after OTA update</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-after-OTA-update/m-p/763476#M118601</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Im trying to get OTA updates on a VAR_SOM_MX6 SOM-Solo running Android 5.0.2 to work, however after (attempting to) applying the update my system is in an unusable state. It cycles between normal mode and recovery mode, I cant use console or adb and therefore cant check logs for what went wrong. Screen output suggests the following problems:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;EXT4-fs (mmcblk1p5): INFO: recovery required on readonly filesystem&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;EXT4-fs (mmcblk1p5): write access will be enabled during recovery&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;EXT4-fs (mmcblk1p5): recovery complete&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;EXT4-fs (mmcblk1p5): mounted filesystem with ordered data mode. Opts: barrier=1&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;fs_mgr: __mount(source=/dev/block/mmcblk1p5,target=/system,type=ext4)=0&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;mmcblk1p5 is mounted readonly. (/dev/block/mmcblk1p5 /system ext4 ro,barrier=1 wait)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;init: cannot execve('/system/bin/displayon.sh'): Permission denied&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;init: cannot execve('/system/bin/lmkd'): Permission denied&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;init: cannot execve('/system/bin/logd'): Permission denied&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;init: cannot execve('/system/bin/servicemanager'): Permission denied&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;init: cannot execve('/system/bin/vold'): Permission denied&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;init: cannot execve('/system/bin/surfaceflinger'): Permission denied&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;...&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;init: critical process 'lmkd' exited 4 times in 4 minutes; rebooting into recovery mode&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This suggests to me the files from the update did get copied but permissions werent set correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What can I do to resolve this issue and get OTA updates to work correctly? Attached are the screen outputs during recovery mode and after the update.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Nov 2017 13:26:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-after-OTA-update/m-p/763476#M118601</guid>
      <dc:creator>saschaseefelder</dc:creator>
      <dc:date>2017-11-10T13:26:42Z</dc:date>
    </item>
    <item>
      <title>Re: Problems after OTA update</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-after-OTA-update/m-p/763477#M118602</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sascha Seefelder,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The VAR-SOM products are supported by Variscite. If the Android image you downloaded on the board is from Variscite’s BSP and does support OTA updates I would recommend contacting them or looking at their forums.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Another alternative would be considering Android-centric forums such as Google’s developer’s portal, as this function changes significantly between Android revisions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Nov 2017 21:13:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-after-OTA-update/m-p/763477#M118602</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2017-11-15T21:13:29Z</dc:date>
    </item>
  </channel>
</rss>