<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Add/Edit source code</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Add-Edit-source-code/m-p/763345#M118561</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Please refer to "i.MX_BSP_Porting_Guide.pdf".&lt;/P&gt;&lt;P&gt;In particular -&amp;nbsp; use Chapter 2 (Porting Kernel) and Chapter 3 (Porting U-Boot).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS" title="https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS"&gt;https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 Jan 2018 08:39:51 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2018-01-29T08:39:51Z</dc:date>
    <item>
      <title>Add/Edit source code</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Add-Edit-source-code/m-p/763344#M118560</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using IMX.7 in combination with Yocto Project.&lt;/P&gt;&lt;P&gt;I follow steps mentioned in&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.yoctoproject.org/docs/2.4.1/mega-manual/mega-manual.html" title="http://www.yoctoproject.org/docs/2.4.1/mega-manual/mega-manual.html"&gt;Yocto Project Mega-Manual&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it took 6 hours on ubuntu to compile bsp and built sd card image.&lt;/P&gt;&lt;P&gt;but didn't understand where to add/edit source code lets say for UART/PCIE etc.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 28 Jan 2018 10:51:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Add-Edit-source-code/m-p/763344#M118560</guid>
      <dc:creator>imx7newbie</dc:creator>
      <dc:date>2018-01-28T10:51:09Z</dc:date>
    </item>
    <item>
      <title>Re: Add/Edit source code</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Add-Edit-source-code/m-p/763345#M118561</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Please refer to "i.MX_BSP_Porting_Guide.pdf".&lt;/P&gt;&lt;P&gt;In particular -&amp;nbsp; use Chapter 2 (Porting Kernel) and Chapter 3 (Porting U-Boot).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS" title="https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS"&gt;https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Jan 2018 08:39:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Add-Edit-source-code/m-p/763345#M118561</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2018-01-29T08:39:51Z</dc:date>
    </item>
  </channel>
</rss>