<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX7 Kernel Config in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Kernel-Config/m-p/763189#M118533</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Linux Kernel v4.9.11_1.0.0_ga commit&amp;nbsp;427eb83 fails to build when only configured for IMX7D SOC. A diff for the kernel configuration patch as attached. Putting this here because the imx kernel repository has no public facing issue tracker.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;gcc version 7.3.0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Compiler Output:&lt;/P&gt;&lt;PRE style="padding-left: 30px;"&gt;drivers/built-in.o: In function `imx7d_charger_primary_detection':
core.c:(.text+0x24df58): undefined reference to `bq2429x_set_ilim'
arch/arm/mach-imx/built-in.o: In function `imx_anatop_pre_suspend':
platform-imx-dma.c:(.text+0xf5c): undefined reference to `imx_gpc_usb_wakeup_enabled'
platform-imx-dma.c:(.text+0xf68): undefined reference to `imx_gpc_enet_wakeup_enabled'
arch/arm/mach-imx/built-in.o: In function `imx_anatop_post_resume':
platform-imx-dma.c:(.text+0x10d0): undefined reference to `imx_gpc_usb_wakeup_enabled'
platform-imx-dma.c:(.text+0x10dc): undefined reference to `imx_gpc_enet_wakeup_enabled'
Makefile:969: recipe for target 'vmlinux' failed
make: *** [vmlinux] Error 1&lt;/PRE&gt;&lt;PRE style="padding-left: 30px;"&gt;&lt;/PRE&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ryan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EDIT:&lt;/P&gt;&lt;P&gt;Building also fails if config option CONFIG_ARM_IMX6Q_CPUFREQ is not set. This should also be fixed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Feb 2018 00:00:16 GMT</pubDate>
    <dc:creator>ryanschaefer</dc:creator>
    <dc:date>2018-02-21T00:00:16Z</dc:date>
    <item>
      <title>i.MX7 Kernel Config</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Kernel-Config/m-p/763189#M118533</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Linux Kernel v4.9.11_1.0.0_ga commit&amp;nbsp;427eb83 fails to build when only configured for IMX7D SOC. A diff for the kernel configuration patch as attached. Putting this here because the imx kernel repository has no public facing issue tracker.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;gcc version 7.3.0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Compiler Output:&lt;/P&gt;&lt;PRE style="padding-left: 30px;"&gt;drivers/built-in.o: In function `imx7d_charger_primary_detection':
core.c:(.text+0x24df58): undefined reference to `bq2429x_set_ilim'
arch/arm/mach-imx/built-in.o: In function `imx_anatop_pre_suspend':
platform-imx-dma.c:(.text+0xf5c): undefined reference to `imx_gpc_usb_wakeup_enabled'
platform-imx-dma.c:(.text+0xf68): undefined reference to `imx_gpc_enet_wakeup_enabled'
arch/arm/mach-imx/built-in.o: In function `imx_anatop_post_resume':
platform-imx-dma.c:(.text+0x10d0): undefined reference to `imx_gpc_usb_wakeup_enabled'
platform-imx-dma.c:(.text+0x10dc): undefined reference to `imx_gpc_enet_wakeup_enabled'
Makefile:969: recipe for target 'vmlinux' failed
make: *** [vmlinux] Error 1&lt;/PRE&gt;&lt;PRE style="padding-left: 30px;"&gt;&lt;/PRE&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ryan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EDIT:&lt;/P&gt;&lt;P&gt;Building also fails if config option CONFIG_ARM_IMX6Q_CPUFREQ is not set. This should also be fixed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Feb 2018 00:00:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Kernel-Config/m-p/763189#M118533</guid>
      <dc:creator>ryanschaefer</dc:creator>
      <dc:date>2018-02-21T00:00:16Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX7 Kernel Config</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Kernel-Config/m-p/763190#M118534</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ryan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please share the link of the git repository where you fetch to download the committ that you are mention?.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Feb 2018 16:14:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Kernel-Config/m-p/763190#M118534</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2018-02-27T16:14:26Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX7 Kernel Config</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Kernel-Config/m-p/763191#M118535</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="link-titled" href="http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/log/?h=imx_4.9.11_1.0.0_ga" title="http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/log/?h=imx_4.9.11_1.0.0_ga"&gt;http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/log/?h=imx_4.9.11_1.0.0_ga&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The commit I shared is the head of freescale provided linux git repository branch imx_4.9.11_1.0.0_ga. I agree that NXP's kernel repositories are not friendly and should be unified.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Feb 2018 16:31:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7-Kernel-Config/m-p/763191#M118535</guid>
      <dc:creator>ryanschaefer</dc:creator>
      <dc:date>2018-02-27T16:31:46Z</dc:date>
    </item>
  </channel>
</rss>