<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックUART2 not working</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/UART2-not-working/m-p/762783#M118471</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Following is the result of loop back test in uart2.&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/18437iE16BE88ABE884B6F/image-size/large?v=v2&amp;amp;px=999" title="uart not working.png" alt="uart not working.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I have used the default configuration in dts file except "&lt;STRONG&gt;fsl,uart-has-rtscts&lt;/STRONG&gt;;"(I commented it). Why it is not working? Whats the error in default configuration?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Feb 2018 11:12:56 GMT</pubDate>
    <dc:creator>mathew_k_t</dc:creator>
    <dc:date>2018-02-21T11:12:56Z</dc:date>
    <item>
      <title>UART2 not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UART2-not-working/m-p/762783#M118471</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Following is the result of loop back test in uart2.&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/18437iE16BE88ABE884B6F/image-size/large?v=v2&amp;amp;px=999" title="uart not working.png" alt="uart not working.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I have used the default configuration in dts file except "&lt;STRONG&gt;fsl,uart-has-rtscts&lt;/STRONG&gt;;"(I commented it). Why it is not working? Whats the error in default configuration?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Feb 2018 11:12:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UART2-not-working/m-p/762783#M118471</guid>
      <dc:creator>mathew_k_t</dc:creator>
      <dc:date>2018-02-21T11:12:56Z</dc:date>
    </item>
    <item>
      <title>Re: UART2 not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UART2-not-working/m-p/762784#M118472</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When you are performing "echo hello" you sending this text into system console and as the console is associated with ttymxc0 UART the text finally arrives at the PC.&lt;BR /&gt;When you are performing "echo hello &amp;gt; /dev/ttymxc0" you sending the data into UART directly as ttymxc0 device not as a console.&lt;BR /&gt;And you are getting the same result. The text arrives at the PC.&lt;BR /&gt;However in case of "echo hello &amp;gt; /dev/ttymxc1" the text goes to UART2 however nothing is listening to UART2 device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Feb 2018 02:29:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UART2-not-working/m-p/762784#M118472</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2018-02-22T02:29:32Z</dc:date>
    </item>
  </channel>
</rss>