<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 i.MX6DL - How many framebuffer can I use?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-How-many-framebuffer-can-I-use/m-p/762646#M118451</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I used I.MX6DL. It has 1 IPU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I used fb0 to camera output. and fb1 to QT's application area.&lt;/P&gt;&lt;P&gt;These are out put to LVDS.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And I can&amp;nbsp;mirroring the fb0 or fb1 to fb2. fb2 is output to External monitor.&amp;nbsp;&lt;/P&gt;&lt;P&gt;But I need 2 of framebuffer (fb0 and fb1 ) output to external monitor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any method to adding the 1 more framebuffer(fb3) in i.MX6DL ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 May 2018 00:36:18 GMT</pubDate>
    <dc:creator>호영노</dc:creator>
    <dc:date>2018-05-17T00:36:18Z</dc:date>
    <item>
      <title>i.MX6DL - How many framebuffer can I use?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-How-many-framebuffer-can-I-use/m-p/762646#M118451</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I used I.MX6DL. It has 1 IPU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I used fb0 to camera output. and fb1 to QT's application area.&lt;/P&gt;&lt;P&gt;These are out put to LVDS.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And I can&amp;nbsp;mirroring the fb0 or fb1 to fb2. fb2 is output to External monitor.&amp;nbsp;&lt;/P&gt;&lt;P&gt;But I need 2 of framebuffer (fb0 and fb1 ) output to external monitor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any method to adding the 1 more framebuffer(fb3) in i.MX6DL ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 May 2018 00:36:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-How-many-framebuffer-can-I-use/m-p/762646#M118451</guid>
      <dc:creator>호영노</dc:creator>
      <dc:date>2018-05-17T00:36:18Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6DL - How many framebuffer can I use?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-How-many-framebuffer-can-I-use/m-p/762647#M118452</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;pls refer to the topic as below, hope helpful for you&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/message/834962?commentID=834962#comment-834962" title="https://community.nxp.com/message/834962?commentID=834962#comment-834962"&gt;https://community.nxp.com/message/834962?commentID=834962#comment-834962&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 May 2018 07:04:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-How-many-framebuffer-can-I-use/m-p/762647#M118452</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-05-17T07:04:42Z</dc:date>
    </item>
  </channel>
</rss>