<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 MEMCPY Problem IMX6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MEMCPY-Problem-IMX6/m-p/761999#M118381</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Im having a problem with the memcpy after initializing the EPIT Driver.&amp;nbsp;&lt;BR /&gt;Does anyone have an idea of what is making the problem?&lt;/P&gt;&lt;P&gt;Im using the u-boot to initialize the board and then use the load and go command to execute the .bin file&lt;/P&gt;&lt;P&gt;Kind regards,&amp;nbsp;&lt;BR /&gt;Ailton Lopes&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Apr 2018 08:16:12 GMT</pubDate>
    <dc:creator>ailtonlopes</dc:creator>
    <dc:date>2018-04-04T08:16:12Z</dc:date>
    <item>
      <title>MEMCPY Problem IMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MEMCPY-Problem-IMX6/m-p/761999#M118381</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Im having a problem with the memcpy after initializing the EPIT Driver.&amp;nbsp;&lt;BR /&gt;Does anyone have an idea of what is making the problem?&lt;/P&gt;&lt;P&gt;Im using the u-boot to initialize the board and then use the load and go command to execute the .bin file&lt;/P&gt;&lt;P&gt;Kind regards,&amp;nbsp;&lt;BR /&gt;Ailton Lopes&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Apr 2018 08:16:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MEMCPY-Problem-IMX6/m-p/761999#M118381</guid>
      <dc:creator>ailtonlopes</dc:creator>
      <dc:date>2018-04-04T08:16:12Z</dc:date>
    </item>
    <item>
      <title>Re: MEMCPY Problem IMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MEMCPY-Problem-IMX6/m-p/762000#M118382</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;what problem do you mean? pls share with me more detailed information, what OS do you use？&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Apr 2018 07:20:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MEMCPY-Problem-IMX6/m-p/762000#M118382</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-04-10T07:20:10Z</dc:date>
    </item>
  </channel>
</rss>