<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic mxc_ipudev_test sample is missing struct ipu_task in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/mxc-ipudev-test-sample-is-missing-struct-ipu-task/m-p/206080#M11838</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all, I have a problem building the mxc_ipudev_test sample in the imx-test suite, looks like there is an undefined structure.&lt;/P&gt;&lt;P&gt;I've tried a complete re-unpack of the imx_test using:&lt;BR /&gt;./ltib -p imx-test -m prep&lt;/P&gt;&lt;P&gt;Then a build using ./ltib yields loads of errors:&lt;/P&gt;&lt;P&gt;make -C mxc_ipudev_test &lt;BR /&gt;make[2]: Entering directory `/home/revo/ltib/rpm/BUILD/imx-test-11.09.01/test/mxc_ipudev_test'&lt;BR /&gt;mkdir -p /home/revo/ltib/rpm/BUILD/imx-test-11.09.01/platform/IMX51/&lt;BR /&gt;In file included from mxc_ipudev_test.c:35:&lt;BR /&gt;mxc_ipudev_test.h:28: error: field 'task' has incomplete type&lt;BR /&gt;mxc_ipudev_test.c: In function 'process_cmdline':&lt;BR /&gt;mxc_ipudev_test.c:56: error: dereferencing pointer to incomplete type&lt;BR /&gt;mxc_ipudev_test.c:56: error: dereferencing pointer to incomplete type&lt;BR /&gt;mxc_ipudev_test.c:57: error: dereferencing pointer to incomplete type&lt;BR /&gt;mxc_ipudev_test.c:58: error: dereferencing pointer to incomplete type&lt;BR /&gt;mxc_ipudev_test.c: In function 'dump_ipu_task':&lt;BR /&gt;mxc_ipudev_test.c:110: error: dereferencing pointer to incomplete type&lt;BR /&gt;mxc_ipudev_test.c:111: error: dereferencing pointer to incomplete type&lt;BR /&gt;............. and many more errors the same.&lt;/P&gt;&lt;P&gt;Looking at file "mxc_ipudev_test.h" line 28 (the first error) it uses an undefined structure "struct ipu_task" which appears to be the root of all these 'incomplete type' errors. But I can't find the declaration of this structure anywhere - I even did a total grep of my hard drive for all files containing the term "ipu_task" but not found. Am I maybe missing an updated header? Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Jan 2012 11:50:17 GMT</pubDate>
    <dc:creator>StevieRG</dc:creator>
    <dc:date>2012-01-27T11:50:17Z</dc:date>
    <item>
      <title>mxc_ipudev_test sample is missing struct ipu_task</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mxc-ipudev-test-sample-is-missing-struct-ipu-task/m-p/206080#M11838</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all, I have a problem building the mxc_ipudev_test sample in the imx-test suite, looks like there is an undefined structure.&lt;/P&gt;&lt;P&gt;I've tried a complete re-unpack of the imx_test using:&lt;BR /&gt;./ltib -p imx-test -m prep&lt;/P&gt;&lt;P&gt;Then a build using ./ltib yields loads of errors:&lt;/P&gt;&lt;P&gt;make -C mxc_ipudev_test &lt;BR /&gt;make[2]: Entering directory `/home/revo/ltib/rpm/BUILD/imx-test-11.09.01/test/mxc_ipudev_test'&lt;BR /&gt;mkdir -p /home/revo/ltib/rpm/BUILD/imx-test-11.09.01/platform/IMX51/&lt;BR /&gt;In file included from mxc_ipudev_test.c:35:&lt;BR /&gt;mxc_ipudev_test.h:28: error: field 'task' has incomplete type&lt;BR /&gt;mxc_ipudev_test.c: In function 'process_cmdline':&lt;BR /&gt;mxc_ipudev_test.c:56: error: dereferencing pointer to incomplete type&lt;BR /&gt;mxc_ipudev_test.c:56: error: dereferencing pointer to incomplete type&lt;BR /&gt;mxc_ipudev_test.c:57: error: dereferencing pointer to incomplete type&lt;BR /&gt;mxc_ipudev_test.c:58: error: dereferencing pointer to incomplete type&lt;BR /&gt;mxc_ipudev_test.c: In function 'dump_ipu_task':&lt;BR /&gt;mxc_ipudev_test.c:110: error: dereferencing pointer to incomplete type&lt;BR /&gt;mxc_ipudev_test.c:111: error: dereferencing pointer to incomplete type&lt;BR /&gt;............. and many more errors the same.&lt;/P&gt;&lt;P&gt;Looking at file "mxc_ipudev_test.h" line 28 (the first error) it uses an undefined structure "struct ipu_task" which appears to be the root of all these 'incomplete type' errors. But I can't find the declaration of this structure anywhere - I even did a total grep of my hard drive for all files containing the term "ipu_task" but not found. Am I maybe missing an updated header? Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jan 2012 11:50:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mxc-ipudev-test-sample-is-missing-struct-ipu-task/m-p/206080#M11838</guid>
      <dc:creator>StevieRG</dc:creator>
      <dc:date>2012-01-27T11:50:17Z</dc:date>
    </item>
    <item>
      <title>Re: mxc_ipudev_test sample is missing struct ipu_task</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mxc-ipudev-test-sample-is-missing-struct-ipu-task/m-p/206081#M11839</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I facing &amp;nbsp;the same issue too&lt;/P&gt;&lt;P&gt;Did you get the resolution?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Mar 2012 03:59:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mxc-ipudev-test-sample-is-missing-struct-ipu-task/m-p/206081#M11839</guid>
      <dc:creator>JackyHuang</dc:creator>
      <dc:date>2012-03-26T03:59:50Z</dc:date>
    </item>
    <item>
      <title>Re: mxc_ipudev_test sample is missing struct ipu_task</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mxc-ipudev-test-sample-is-missing-struct-ipu-task/m-p/206082#M11840</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi @jacky, sorry no I did not get a fix for this, I'd be grateful if anyone does have a fix though and could help us out.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Mar 2012 07:24:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mxc-ipudev-test-sample-is-missing-struct-ipu-task/m-p/206082#M11840</guid>
      <dc:creator>StevieRG</dc:creator>
      <dc:date>2012-03-26T07:24:50Z</dc:date>
    </item>
    <item>
      <title>Re: mxc_ipudev_test sample is missing struct ipu_task</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mxc-ipudev-test-sample-is-missing-struct-ipu-task/m-p/206083#M11841</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I looked at this a while ago. In the end I reverse engineered the declaration of "struct ipu_task" by looking at how it is used in the function dump_ipu_task() in file mxc_ipudev_test.c, but couldn't be confident of the right member ordering.&lt;/P&gt;&lt;P&gt;However, in general I found because of the lack of information on how to use the IPU interface via the "file descriptor and ioctl" method used in that example, I chose to use the IPU examples from the previous BSP instead, which are much better documented and work very well. I can make the IPU do pretty well anything using this older method. I converted the previous BSP examples to build under the new (11.09) BSP and posted them here, if they are useful to you:&lt;/P&gt;&lt;P&gt;&lt;A href="http://imxcommunity.org/group/graphics-display/forum/topics/info-using-older-mxc-ipudev-test-on-newer-bsp" rel="nofollow" target="_self"&gt;http://imxcommunity.org/group/graphics-display/forum/topics/info-us...&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jul 2012 14:31:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mxc-ipudev-test-sample-is-missing-struct-ipu-task/m-p/206083#M11841</guid>
      <dc:creator>StevieRG</dc:creator>
      <dc:date>2012-07-04T14:31:51Z</dc:date>
    </item>
  </channel>
</rss>