<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: fb is not supported for imx8mqevk in L4.9.51_imx8mq-ga</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/fb-is-not-supported-for-imx8mqevk-in-L4-9-51-imx8mq-ga/m-p/761971#M118376</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;yes, current bsp only supports wayland.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Apr 2018 07:13:22 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2018-04-10T07:13:22Z</dc:date>
    <item>
      <title>fb is not supported for imx8mqevk in L4.9.51_imx8mq-ga</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/fb-is-not-supported-for-imx8mqevk-in-L4-9-51-imx8mq-ga/m-p/761967#M118372</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I was trying to build an image to framebuffer with the new release for my&amp;nbsp;imx8mqevk demoboard without luck. The steps I've done:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;$ DISTRO=fsl-imx-fb MACHINE=imx8mqevk source fsl-setup-release.sh –b build-fb&lt;/P&gt;&lt;P&gt;$ bitbake imx-gpu-viv&lt;/P&gt;&lt;P&gt;Loading cache: 100% |###################################################################################################################################################| Time: 0:00:01&lt;BR /&gt;Loaded 3068 entries from dependency cache.&lt;BR /&gt;ERROR: Nothing PROVIDES 'imx-gpu-viv'&lt;BR /&gt;ERROR: imx-gpu-viv was skipped: incompatible with machine imx8mqevk (not in COMPATIBLE_MACHINE)&lt;BR /&gt;ERROR: imx-gpu-viv was skipped: incompatible with machine imx8mqevk (not in COMPATIBLE_MACHINE)&lt;BR /&gt;ERROR: imx-gpu-viv was skipped: You must set MACHINE_SOCARCH_SUFFIX as MACHINE_SOCARCH_FILTER is set for this SoC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The same steps with the L4.9.51_imx8mq-beta release worked ok.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any solution?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Apr 2018 07:57:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/fb-is-not-supported-for-imx8mqevk-in-L4-9-51-imx8mq-ga/m-p/761967#M118372</guid>
      <dc:creator>_andev_</dc:creator>
      <dc:date>2018-04-04T07:57:06Z</dc:date>
    </item>
    <item>
      <title>Re: fb is not supported for imx8mqevk in L4.9.51_imx8mq-ga</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/fb-is-not-supported-for-imx8mqevk-in-L4-9-51-imx8mq-ga/m-p/761968#M118373</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've been&lt;STRONG&gt; &lt;/STRONG&gt;able to track down the problem to the file:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;sources/meta-freescale/conf/machine/include/imx-base.inc&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the previous version this file didn't exist. If I remove that file I can build the image. I guess the mx8 definitions are missing in this file...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Apr 2018 09:38:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/fb-is-not-supported-for-imx8mqevk-in-L4-9-51-imx8mq-ga/m-p/761968#M118373</guid>
      <dc:creator>_andev_</dc:creator>
      <dc:date>2018-04-04T09:38:06Z</dc:date>
    </item>
    <item>
      <title>Re: fb is not supported for imx8mqevk in L4.9.51_imx8mq-ga</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/fb-is-not-supported-for-imx8mqevk-in-L4-9-51-imx8mq-ga/m-p/761969#M118374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There doesn't seem to be framebuffer (or X11) support as per&amp;nbsp;L4.9.51_imx8mq-ga release notes :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No X11 backend is supported in i.MX 8MQuad.&lt;BR /&gt;No Frame Buffer backend is supported in i.MX 8MQuad.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The only option is building for wayland, similar question in this &lt;A _jive_internal="true" href="https://community.nxp.com/thread/472956"&gt;thread&lt;/A&gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Apr 2018 10:29:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/fb-is-not-supported-for-imx8mqevk-in-L4-9-51-imx8mq-ga/m-p/761969#M118374</guid>
      <dc:creator>mtx512</dc:creator>
      <dc:date>2018-04-04T10:29:58Z</dc:date>
    </item>
    <item>
      <title>Re: fb is not supported for imx8mqevk in L4.9.51_imx8mq-ga</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/fb-is-not-supported-for-imx8mqevk-in-L4-9-51-imx8mq-ga/m-p/761970#M118375</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, you're right. Now I've arrived until the cairo recipe building problem like described in the thread you linked.&lt;/P&gt;&lt;P&gt;We'll need to wait to NXP to patch this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your answer.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Apr 2018 10:55:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/fb-is-not-supported-for-imx8mqevk-in-L4-9-51-imx8mq-ga/m-p/761970#M118375</guid>
      <dc:creator>_andev_</dc:creator>
      <dc:date>2018-04-04T10:55:53Z</dc:date>
    </item>
    <item>
      <title>Re: fb is not supported for imx8mqevk in L4.9.51_imx8mq-ga</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/fb-is-not-supported-for-imx8mqevk-in-L4-9-51-imx8mq-ga/m-p/761971#M118376</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;yes, current bsp only supports wayland.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Apr 2018 07:13:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/fb-is-not-supported-for-imx8mqevk-in-L4-9-51-imx8mq-ga/m-p/761971#M118376</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-04-10T07:13:22Z</dc:date>
    </item>
    <item>
      <title>Re: fb is not supported for imx8mqevk in L4.9.51_imx8mq-ga</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/fb-is-not-supported-for-imx8mqevk-in-L4-9-51-imx8mq-ga/m-p/761972#M118377</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are there plans for the bsp to support fbdev or moving to DRM ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Apr 2018 18:46:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/fb-is-not-supported-for-imx8mqevk-in-L4-9-51-imx8mq-ga/m-p/761972#M118377</guid>
      <dc:creator>mtx512</dc:creator>
      <dc:date>2018-04-10T18:46:11Z</dc:date>
    </item>
  </channel>
</rss>