<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Unknown delay during boot (i.mx253) when DMA is enabled.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Unknown-delay-during-boot-i-mx253-when-DMA-is-enabled/m-p/206027#M11830</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could this help?&lt;/P&gt;&lt;P&gt;&lt;A href="http://sw-git.freescale.net/cgi-bin/gitweb.cgi?p=linux-2.6-imx.git;a=commit;h=c037ead48aeb3cbc54fb15d0039ba779eaa6fe65" title="http://sw-git.freescale.net/cgi-bin/gitweb.cgi?p=linux-2.6-imx.git;a=commit;h=c037ead48aeb3cbc54fb15d0039ba779eaa6fe65"&gt;http://sw-git.freescale.net/cgi-bin/gitweb.cgi?p=linux-2.6-imx.git;a=commit;h=c037ead48aeb3cbc54fb15d0039ba779eaa6fe65&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 Oct 2012 15:47:28 GMT</pubDate>
    <dc:creator>FlorentAuger</dc:creator>
    <dc:date>2012-10-29T15:47:28Z</dc:date>
    <item>
      <title>Unknown delay during boot (i.mx253) when DMA is enabled.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unknown-delay-during-boot-i-mx253-when-DMA-is-enabled/m-p/206024#M11827</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi folks.&lt;/P&gt;&lt;P&gt;On your custom board based on i.mx253 running a stock 2.6.39.4 kernel, i've noticed a strange behavior when DMA is enabled.&lt;/P&gt;&lt;P&gt;For some reason the booting stalls for ~60s, and resumes without any error and/or warnings.&lt;/P&gt;&lt;P&gt;From what i could find out, the DMA in mx25 is the same as in mx35. I'm using a firmware originally designed for mx35 with the 2.6.39.4 kernel, "stock defaults" with the 3.x.x kernels.&lt;/P&gt;&lt;P&gt;I've tried different kernels; 3.0.8, 3.1.2, 3.2.0 all behaving the same way...&lt;/P&gt;&lt;P&gt;Is this a normal behavior? Am i doing something wrong, am i missing something?&lt;/P&gt;&lt;P&gt;Is there a way to improve the speed?&lt;/P&gt;&lt;P&gt;&amp;lt;snip&amp;gt;&lt;/P&gt;&lt;P&gt;[ &amp;nbsp;&amp;nbsp; 3.386247] mousedev: PS/2 mouse device common for all mice&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.390370] input: gpio-keys as /devices/platform/gpio-keys/input/input0&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.397442] input: TSC2007 Touchscreen as /devices/virtual/input/input1&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.404424] rtc-ds1307 0-0068: SET TIME!&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.409180] rtc-ds1307 0-0068: rtc core: registered ds1339 as rtc0&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.413267] i2c /dev entries driver&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 64.181134] imx-sdma imx-sdma: initialized&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 64.184593] sdhci: Secure Digital Host Controller Interface driver&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 64.188044] sdhci: Copyright(c) Pierre Ossman&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 64.190758] _regulator_get: sdhci-esdhc-imx.1 supply vmmc not found, using dummy regulator&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 64.196746] mmc0: SDHCI controller on platform [sdhci-esdhc-imx.1] using DMA&lt;/P&gt;&lt;P&gt;&amp;lt;/snip&amp;gt;&lt;/P&gt;&lt;P&gt;Thanx for your help in advance.&lt;/P&gt;&lt;P&gt;Cheers, Kardy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jan 2012 14:57:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unknown-delay-during-boot-i-mx253-when-DMA-is-enabled/m-p/206024#M11827</guid>
      <dc:creator>PeterKardos</dc:creator>
      <dc:date>2012-01-26T14:57:56Z</dc:date>
    </item>
    <item>
      <title>Re: Unknown delay during boot (i.mx253) when DMA is enabled.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unknown-delay-during-boot-i-mx253-when-DMA-is-enabled/m-p/206025#M11828</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Kardy,&lt;/P&gt;&lt;P&gt;if it happens with 3.2.0 as well, I'd say it is a bug and should be reported on the ARM Linux Kernel mailinglist, with Cc: to kernel@pengutronix.de. I don't remember having seen anything like this on the mainline before. You could try to disable some of the drivers "around" the breakage (which is i2c and imx-sdma) and check if it is really the sdma driver.&lt;/P&gt;&lt;P&gt;rsc&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jan 2012 15:06:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unknown-delay-during-boot-i-mx253-when-DMA-is-enabled/m-p/206025#M11828</guid>
      <dc:creator>RobertSchwebel</dc:creator>
      <dc:date>2012-01-26T15:06:09Z</dc:date>
    </item>
    <item>
      <title>Re: Unknown delay during boot (i.mx253) when DMA is enabled.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unknown-delay-during-boot-i-mx253-when-DMA-is-enabled/m-p/206026#M11829</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Robert,&lt;/P&gt;&lt;P&gt;It seem to be only DMA related. If i disable DMA (kernel config=&amp;gt;Device Drivers=&amp;gt;DMA engine support), then the kernel starts within ~5s...&lt;/P&gt;&lt;P&gt;It could be that the firmware is "not the right fit" (even thou it should be compatible). Is there a tool for generating the FW?&lt;/P&gt;&lt;P&gt;-Kardy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jan 2012 15:19:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unknown-delay-during-boot-i-mx253-when-DMA-is-enabled/m-p/206026#M11829</guid>
      <dc:creator>PeterKardos</dc:creator>
      <dc:date>2012-01-26T15:19:29Z</dc:date>
    </item>
    <item>
      <title>Re: Unknown delay during boot (i.mx253) when DMA is enabled.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unknown-delay-during-boot-i-mx253-when-DMA-is-enabled/m-p/206027#M11830</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could this help?&lt;/P&gt;&lt;P&gt;&lt;A href="http://sw-git.freescale.net/cgi-bin/gitweb.cgi?p=linux-2.6-imx.git;a=commit;h=c037ead48aeb3cbc54fb15d0039ba779eaa6fe65" title="http://sw-git.freescale.net/cgi-bin/gitweb.cgi?p=linux-2.6-imx.git;a=commit;h=c037ead48aeb3cbc54fb15d0039ba779eaa6fe65"&gt;http://sw-git.freescale.net/cgi-bin/gitweb.cgi?p=linux-2.6-imx.git;a=commit;h=c037ead48aeb3cbc54fb15d0039ba779eaa6fe65&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Oct 2012 15:47:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unknown-delay-during-boot-i-mx253-when-DMA-is-enabled/m-p/206027#M11830</guid>
      <dc:creator>FlorentAuger</dc:creator>
      <dc:date>2012-10-29T15:47:28Z</dc:date>
    </item>
    <item>
      <title>Re: Unknown delay during boot (i.mx253) when DMA is enabled.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unknown-delay-during-boot-i-mx253-when-DMA-is-enabled/m-p/206028#M11831</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, there is a tool for generating the the sdma firmware that the mainline kernel requires at:&lt;/P&gt;&lt;P&gt;&lt;A href="http://git.pengutronix.de/?p=imx/sdma-firmware.git;a=summary" title="http://git.pengutronix.de/?p=imx/sdma-firmware.git;a=summary"&gt;http://git.pengutronix.de/?p=imx/sdma-firmware.git;a=summary&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you provide the firmware generated by this tool, you will not experience the long wait timeout.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fabio Estevam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Oct 2012 16:08:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unknown-delay-during-boot-i-mx253-when-DMA-is-enabled/m-p/206028#M11831</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2012-10-29T16:08:47Z</dc:date>
    </item>
  </channel>
</rss>