<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Reading from GPIO_PSR/DR</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Reading-from-GPIO-PSR-DR/m-p/761508#M118299</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; look at the following &lt;A href="https://community.nxp.com/message/304791"&gt;https://community.nxp.com/message/304791&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Apr 2018 08:56:10 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2018-04-04T08:56:10Z</dc:date>
    <item>
      <title>Reading from GPIO_PSR/DR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reading-from-GPIO-PSR-DR/m-p/761507#M118298</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a&amp;nbsp;question with the GPIO Read Mode sequence. After writing value to data_register (GPIO_DR), should be able to read the same state from the GPIO_PSR after I have configured GPIO direction register to input? I saw that reading in input mode, the value from GPIO_DR is updated after I wrote something, but this is not the case for GPIO_PSR.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Apr 2018 15:05:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reading-from-GPIO-PSR-DR/m-p/761507#M118298</guid>
      <dc:creator>adelindobre</dc:creator>
      <dc:date>2018-04-03T15:05:28Z</dc:date>
    </item>
    <item>
      <title>Re: Reading from GPIO_PSR/DR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reading-from-GPIO-PSR-DR/m-p/761508#M118299</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; look at the following &lt;A href="https://community.nxp.com/message/304791"&gt;https://community.nxp.com/message/304791&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Apr 2018 08:56:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reading-from-GPIO-PSR-DR/m-p/761508#M118299</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2018-04-04T08:56:10Z</dc:date>
    </item>
  </channel>
</rss>