<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックKeep boot logo from bootloader when kernel is loaded in LVDS display</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Keep-boot-logo-from-bootloader-when-kernel-is-loaded-in-LVDS/m-p/761202#M118272</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using IMX6Q with barebox v2016.11.0&amp;nbsp; and linux kernel v4.1.36. I using LVDS display with custom logo both in the bootloader and kernel. When switching from bootloader to kernel the image gets distorted and sets back when the imx-drm drivers are loaded. I would like to know how to solve this issue. Kindly guide me to solve this issue.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Apr 2018 10:33:19 GMT</pubDate>
    <dc:creator>bhamynarasimhas</dc:creator>
    <dc:date>2018-04-24T10:33:19Z</dc:date>
    <item>
      <title>Keep boot logo from bootloader when kernel is loaded in LVDS display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Keep-boot-logo-from-bootloader-when-kernel-is-loaded-in-LVDS/m-p/761202#M118272</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using IMX6Q with barebox v2016.11.0&amp;nbsp; and linux kernel v4.1.36. I using LVDS display with custom logo both in the bootloader and kernel. When switching from bootloader to kernel the image gets distorted and sets back when the imx-drm drivers are loaded. I would like to know how to solve this issue. Kindly guide me to solve this issue.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Apr 2018 10:33:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Keep-boot-logo-from-bootloader-when-kernel-is-loaded-in-LVDS/m-p/761202#M118272</guid>
      <dc:creator>bhamynarasimhas</dc:creator>
      <dc:date>2018-04-24T10:33:19Z</dc:date>
    </item>
    <item>
      <title>Re: Keep boot logo from bootloader when kernel is loaded in LVDS display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Keep-boot-logo-from-bootloader-when-kernel-is-loaded-in-LVDS/m-p/761203#M118273</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bhamy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The issues is barebox, can´t not parse device tree, Let the imx-ldb.c code in the kernel to probe and *add* a way to parse the device-tree for adding mode timing property using the display-timing stuff. (this means kernel patch)&lt;/P&gt;&lt;P&gt;or Look for a common timings from an existing displays in simple-panel.c and pass them to the compatibile property of the panel in the device-tree via bootloader. however unfortunately barebox is not supported.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Apr 2018 13:54:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Keep-boot-logo-from-bootloader-when-kernel-is-loaded-in-LVDS/m-p/761203#M118273</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2018-04-25T13:54:04Z</dc:date>
    </item>
  </channel>
</rss>