<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.mx6ull feature version pin compatibility</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6ull-feature-version-pin-compatibility/m-p/760730#M118209</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;They are compatible, but with 1G RAM you should modify the uboot source code and adapt it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 21 May 2018 14:24:57 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2018-05-21T14:24:57Z</dc:date>
    <item>
      <title>i.mx6ull feature version pin compatibility</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6ull-feature-version-pin-compatibility/m-p/760729#M118208</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;NXP doesn't provide schematic symbols or footprints, so I'm about to have to put a lot of work into creating my Altium symbol (all 289 pins) for the i.mx6ull and what I'm wondering is whether the part numbers between feature sets (e.g.,&amp;nbsp;MCIMX6Y2CVK08AB vs. the&amp;nbsp;MCIMX6Y2CVK05AB) are drop-in pin compatible.&amp;nbsp; The only difference I see is the max speed (05 is 528MHz and 08 is 792MHz).&amp;nbsp; The speed doesn't matter to me anyway because i'm going to dial it back as far as I can while still getting linux to run in order to minimize power consumption.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Speaking of linux, I'm planning to base my board on the eval board reference design from the i.mx6ull product page.&amp;nbsp; There's a linux download and yocto project and what I'm wondering is, since the eval board runs the&amp;nbsp;MCIMX6Y2DVM05AA which is the commercial temperature instead of industrial temperature and 528MHz, when i lay out my new board will the pre-compiled linux image that was built for the eval kit work with my board?&amp;nbsp; Would linux care or even notice that the model number isn't the same?&amp;nbsp; Along those same lines, the eval board uses 4Gb DDR3L RAM and I was looking to use 1Gb DDR3L RAM instead because it's way cheaper and more readily available. Other than potential performance issues (I'm ultimately not even going to run a desktop on my device, just a single executable that is the GUI for the device), will Linux care that the ram size is different? The RAM i'm looking at is pin-compatible and is the same x16 format as what's on the eval board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 May 2018 13:03:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6ull-feature-version-pin-compatibility/m-p/760729#M118208</guid>
      <dc:creator>dluberger</dc:creator>
      <dc:date>2018-05-16T13:03:59Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6ull feature version pin compatibility</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6ull-feature-version-pin-compatibility/m-p/760730#M118209</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;They are compatible, but with 1G RAM you should modify the uboot source code and adapt it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 May 2018 14:24:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6ull-feature-version-pin-compatibility/m-p/760730#M118209</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2018-05-21T14:24:57Z</dc:date>
    </item>
  </channel>
</rss>