<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to disable Temperature Limit in iMX6 CPU Single Core in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-disable-Temperature-Limit-in-iMX6-CPU-Single-Core/m-p/760098#M118131</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we are using iMX6 CPU single Core, at room temperature(25 C) we read die temperature is 57 C , and No application is running this time except Linux OS. and I believe after 85 C CPU fold-back the its clock when temperature hit the set 85 C,Correct me if i am wrong here.&lt;/P&gt;&lt;P&gt;first Why the temperature is high even i am not running any application, second why alarm&amp;nbsp;point is set 85 C (die temp)&lt;/P&gt;&lt;P&gt;its too low, because i hit 57 C at room &amp;nbsp;temperature, and in real world it I run this to 65 C ambient , the temperature will go more than 85C ( without running any application) and clock will reduce so hence performance, Correct me here too if i am wrong.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And last if I need to increase its core temperature limit 85 C to (MAX -10C) , Let me know how it can be done in Linux.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 Feb 2018 09:13:09 GMT</pubDate>
    <dc:creator>kunalbarot</dc:creator>
    <dc:date>2018-02-20T09:13:09Z</dc:date>
    <item>
      <title>How to disable Temperature Limit in iMX6 CPU Single Core</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-disable-Temperature-Limit-in-iMX6-CPU-Single-Core/m-p/760098#M118131</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we are using iMX6 CPU single Core, at room temperature(25 C) we read die temperature is 57 C , and No application is running this time except Linux OS. and I believe after 85 C CPU fold-back the its clock when temperature hit the set 85 C,Correct me if i am wrong here.&lt;/P&gt;&lt;P&gt;first Why the temperature is high even i am not running any application, second why alarm&amp;nbsp;point is set 85 C (die temp)&lt;/P&gt;&lt;P&gt;its too low, because i hit 57 C at room &amp;nbsp;temperature, and in real world it I run this to 65 C ambient , the temperature will go more than 85C ( without running any application) and clock will reduce so hence performance, Correct me here too if i am wrong.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And last if I need to increase its core temperature limit 85 C to (MAX -10C) , Let me know how it can be done in Linux.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Feb 2018 09:13:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-disable-Temperature-Limit-in-iMX6-CPU-Single-Core/m-p/760098#M118131</guid>
      <dc:creator>kunalbarot</dc:creator>
      <dc:date>2018-02-20T09:13:09Z</dc:date>
    </item>
    <item>
      <title>Re: How to disable Temperature Limit in iMX6 CPU Single Core</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-disable-Temperature-Limit-in-iMX6-CPU-Single-Core/m-p/760099#M118132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kunal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please check AN4579 i.MX 6 Series Thermal Management Guidelines&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN4579.pdf" title="https://www.nxp.com/docs/en/application-note/AN4579.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN4579.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and description of thermal driver in Chapter 25 Thermal Driver attached Linux Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Feb 2018 22:59:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-disable-Temperature-Limit-in-iMX6-CPU-Single-Core/m-p/760099#M118132</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-02-20T22:59:15Z</dc:date>
    </item>
  </channel>
</rss>