<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Framebuffer rotation 90 degrees in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Framebuffer-rotation-90-degrees/m-p/760097#M118130</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I find some ipu example, hope helpful for you&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/rogeriorps/ipu-examples" title="https://github.com/rogeriorps/ipu-examples"&gt;GitHub - rogeriorps/ipu-examples: IPU example codes for i.MX5 and i.MX6 families&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-94961"&gt;https://community.nxp.com/docs/DOC-94961&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 Jun 2018 08:07:25 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2018-06-11T08:07:25Z</dc:date>
    <item>
      <title>Framebuffer rotation 90 degrees</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Framebuffer-rotation-90-degrees/m-p/760096#M118129</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have an application running on customized i.MX6 using DirectFB for displaying images.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We now have a requirement of converting to portrait mode, currently the LCD is in landscape mode.. So , we want the image to be displayed 90 degrees rotated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DirectFB only supports 180 degree rotation, If i pass "layer-rotate=90" or "layer-rotate=270", it throws error: "UNIMPLEMENTED".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried the rotation example from IPU examples, but it was rotating one image.. Now suppose if I want to use this IPU code and add it into the DirectFB for frame buffer rotation of 90 degrees.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jun 2018 04:04:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Framebuffer-rotation-90-degrees/m-p/760096#M118129</guid>
      <dc:creator>jamalmohiuddin</dc:creator>
      <dc:date>2018-06-07T04:04:08Z</dc:date>
    </item>
    <item>
      <title>Re: Framebuffer rotation 90 degrees</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Framebuffer-rotation-90-degrees/m-p/760097#M118130</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I find some ipu example, hope helpful for you&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/rogeriorps/ipu-examples" title="https://github.com/rogeriorps/ipu-examples"&gt;GitHub - rogeriorps/ipu-examples: IPU example codes for i.MX5 and i.MX6 families&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-94961"&gt;https://community.nxp.com/docs/DOC-94961&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jun 2018 08:07:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Framebuffer-rotation-90-degrees/m-p/760097#M118130</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-06-11T08:07:25Z</dc:date>
    </item>
  </channel>
</rss>