<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ECSPI DMA support for MAX14830 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ECSPI-DMA-support-for-MAX14830/m-p/759836#M118102</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Surendra&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;sdma may not help with with overrun, recommended to use flow control.&lt;/P&gt;&lt;P&gt;As for spi dma support, it is not supported in nxp linux bsps according to attached Linux&lt;/P&gt;&lt;P&gt;Manual sect.4.1.2 Software Operation.&lt;/P&gt;&lt;P&gt;In general one can just follow documentation in linux/Documentation/devicetree/bindings/spi/fsl-imx-cspi.txt&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/Documentation/devicetree/bindings/spi/fsl-imx-cspi.txt?h=imx_4.1.15_2.0.0_ga&amp;amp;id=rel_imx_4.1.15_2.0.0_ga" title="http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/Documentation/devicetree/bindings/spi/fsl-imx-cspi.txt?h=imx_4.1.15_2.0.0_ga&amp;amp;id=rel_imx_4.1.15_2.0.0_ga"&gt;linux-imx.git - i.MX Linux Kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Jan 2018 07:43:26 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-01-03T07:43:26Z</dc:date>
    <item>
      <title>ECSPI DMA support for MAX14830</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ECSPI-DMA-support-for-MAX14830/m-p/759835#M118101</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; As we facing the issue of the rxoverrun for spi-uart exapnder chip 14830, looking for the use of DMA for the same so that cpu overhead will reduce and communication will be faster.&lt;/P&gt;&lt;P&gt;Then we will check the ovevrrun is happening or not for MAX14830.&lt;/P&gt;&lt;P&gt;What could be the approach to use DMA ?&lt;/P&gt;&lt;P&gt;I have enabled dma for the ecspi. but still it&amp;nbsp;using the pio mode in the spi-imx driver.&lt;/P&gt;&lt;P&gt;As max14830 is slave&amp;nbsp;device in the communication, is we need to implement anything in max310x driver for the DMA burst mechanism ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Surendra&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jan 2018 05:02:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ECSPI-DMA-support-for-MAX14830/m-p/759835#M118101</guid>
      <dc:creator>surendradhobale</dc:creator>
      <dc:date>2018-01-03T05:02:58Z</dc:date>
    </item>
    <item>
      <title>Re: ECSPI DMA support for MAX14830</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ECSPI-DMA-support-for-MAX14830/m-p/759836#M118102</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Surendra&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;sdma may not help with with overrun, recommended to use flow control.&lt;/P&gt;&lt;P&gt;As for spi dma support, it is not supported in nxp linux bsps according to attached Linux&lt;/P&gt;&lt;P&gt;Manual sect.4.1.2 Software Operation.&lt;/P&gt;&lt;P&gt;In general one can just follow documentation in linux/Documentation/devicetree/bindings/spi/fsl-imx-cspi.txt&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/Documentation/devicetree/bindings/spi/fsl-imx-cspi.txt?h=imx_4.1.15_2.0.0_ga&amp;amp;id=rel_imx_4.1.15_2.0.0_ga" title="http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/Documentation/devicetree/bindings/spi/fsl-imx-cspi.txt?h=imx_4.1.15_2.0.0_ga&amp;amp;id=rel_imx_4.1.15_2.0.0_ga"&gt;linux-imx.git - i.MX Linux Kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jan 2018 07:43:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ECSPI-DMA-support-for-MAX14830/m-p/759836#M118102</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-01-03T07:43:26Z</dc:date>
    </item>
  </channel>
</rss>