<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimx53 MFGtool error when using plugin-based U-Boot</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx53-MFGtool-error-when-using-plugin-based-U-Boot/m-p/758756#M117970</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have an iMX53-based platform that uses the DCD approach in U-Boot to perform device configuring both for the production and manufacturing versions of U-Boot and we have been successfully using the Freescale MFGTool (using the manufacturing version of U-Boot) to program the boards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have now changed to use the plugin approach to configure the device for both production and manufacturing versions of U-Boot. The production U-Boot works and the board boots correctly. However the MFGTool fails straightway when attempting to program the board using the new plugin-based U-boot approach.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone know of any issues relating to the use the MFGTool when using the iMX53 plugin approach?&lt;/P&gt;&lt;P&gt;Does the xml file differ between the DCD and plugin approaches - we use the same xml file for both. I've attached a copy of the xml file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MfgTool version is V1.6.2.055.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Bruno&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here's the relevant error from the MfgTool log&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Monday, December 04, 2017 12:52:13&lt;BR /&gt;1 - Panel A Start processing BT500-V4 &amp;lt;LIST/&amp;gt;.&lt;BR /&gt;&lt;BR /&gt;Panel A Start &amp;lt;CMD/&amp;gt; type="boot" body="BootStrap" file="u-boot-mfg.bin" timeout="10" onError="" text=" Boot from mfg-mode U-Boot ".&lt;BR /&gt;&lt;BR /&gt;1 - Panel A DoBoot() - Failed to load u-boot-mfg.bin to Recovery mode device. (err=6)&lt;BR /&gt;&lt;BR /&gt;1 - Panel A Finished &amp;lt;CMD/&amp;gt; type="boot" body="BootStrap" file="u-boot-mfg.bin" timeout="10" onError="" text=" Boot from mfg-mode U-Boot " FAIL code=0x6.&lt;BR /&gt;&lt;BR /&gt;Panel A: Reason is unknown,failed to run command: type="boot" body="BootStrap" file="u-boot-mfg.bin" timeout="10" onError="" text=" Boot from mfg-mode U-Boot "&amp;nbsp; The handle is invalid.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;2 - Panel A Finished processing BT500-V4 &amp;lt;LIST/&amp;gt; : FAIL code=6.&lt;BR /&gt;&lt;BR /&gt;Panel A: Reason is unknown,Operation stopped by user. The process terminated unexpectedly.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 04 Dec 2017 14:29:48 GMT</pubDate>
    <dc:creator>bdp42</dc:creator>
    <dc:date>2017-12-04T14:29:48Z</dc:date>
    <item>
      <title>imx53 MFGtool error when using plugin-based U-Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx53-MFGtool-error-when-using-plugin-based-U-Boot/m-p/758756#M117970</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have an iMX53-based platform that uses the DCD approach in U-Boot to perform device configuring both for the production and manufacturing versions of U-Boot and we have been successfully using the Freescale MFGTool (using the manufacturing version of U-Boot) to program the boards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have now changed to use the plugin approach to configure the device for both production and manufacturing versions of U-Boot. The production U-Boot works and the board boots correctly. However the MFGTool fails straightway when attempting to program the board using the new plugin-based U-boot approach.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone know of any issues relating to the use the MFGTool when using the iMX53 plugin approach?&lt;/P&gt;&lt;P&gt;Does the xml file differ between the DCD and plugin approaches - we use the same xml file for both. I've attached a copy of the xml file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MfgTool version is V1.6.2.055.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Bruno&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here's the relevant error from the MfgTool log&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Monday, December 04, 2017 12:52:13&lt;BR /&gt;1 - Panel A Start processing BT500-V4 &amp;lt;LIST/&amp;gt;.&lt;BR /&gt;&lt;BR /&gt;Panel A Start &amp;lt;CMD/&amp;gt; type="boot" body="BootStrap" file="u-boot-mfg.bin" timeout="10" onError="" text=" Boot from mfg-mode U-Boot ".&lt;BR /&gt;&lt;BR /&gt;1 - Panel A DoBoot() - Failed to load u-boot-mfg.bin to Recovery mode device. (err=6)&lt;BR /&gt;&lt;BR /&gt;1 - Panel A Finished &amp;lt;CMD/&amp;gt; type="boot" body="BootStrap" file="u-boot-mfg.bin" timeout="10" onError="" text=" Boot from mfg-mode U-Boot " FAIL code=0x6.&lt;BR /&gt;&lt;BR /&gt;Panel A: Reason is unknown,failed to run command: type="boot" body="BootStrap" file="u-boot-mfg.bin" timeout="10" onError="" text=" Boot from mfg-mode U-Boot "&amp;nbsp; The handle is invalid.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;2 - Panel A Finished processing BT500-V4 &amp;lt;LIST/&amp;gt; : FAIL code=6.&lt;BR /&gt;&lt;BR /&gt;Panel A: Reason is unknown,Operation stopped by user. The process terminated unexpectedly.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Dec 2017 14:29:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx53-MFGtool-error-when-using-plugin-based-U-Boot/m-p/758756#M117970</guid>
      <dc:creator>bdp42</dc:creator>
      <dc:date>2017-12-04T14:29:48Z</dc:date>
    </item>
    <item>
      <title>Re: imx53 MFGtool error when using plugin-based U-Boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx53-MFGtool-error-when-using-plugin-based-U-Boot/m-p/758757#M117971</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;what is the meaning of "plugin" approach?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Dec 2017 01:43:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx53-MFGtool-error-when-using-plugin-based-U-Boot/m-p/758757#M117971</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2017-12-18T01:43:01Z</dc:date>
    </item>
  </channel>
</rss>