<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RGMII_RX_CTL cannot output high level signal when configured as GPIO in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RGMII-RX-CTL-cannot-output-high-level-signal-when-configured-as/m-p/758311#M117918</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shawn&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is there some rgmii circuit on the board, as for example on i.MX6QP Sabre SD schematic SPF-28857&lt;BR /&gt;these two signals are connected to outputs of AR8031 (U516) RGMII_RXD3, RGMII_RXDV.&lt;BR /&gt;In general one can attach jtag and check iomux settings and try manually set them to '1' signal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 May 2018 01:12:21 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-05-17T01:12:21Z</dc:date>
    <item>
      <title>RGMII_RX_CTL cannot output high level signal when configured as GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RGMII-RX-CTL-cannot-output-high-level-signal-when-configured-as/m-p/758310#M117917</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt; color: black;"&gt;Hi FSL engineer,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt; color: black;"&gt;I want the pins RGMII_RX_CTL and RGMII_RD3 work as GPIO(output only). And the other signals for these pins were commented. Finally the pin cannot out '1' signal and always keep low. But I replace the pins with GPIO_7 and GPIO_8. It works normally.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt; color: black;"&gt;I checked the RM and cannot find the difference between these two pairs of pins when configured as GPIO. Could you please advise me how to fix this issue? Thank you.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt; color: black;"&gt;/***********************************************************/&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt; color: black;"&gt;SoC:i.MX 6QP, OS: M6.0&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt; color: black;"&gt;MX6QDL_PAD_RGMII_RX_CTL__GPIO6_IO24&amp;nbsp; 0x00013030&amp;nbsp;&lt;BR /&gt;MX6QDL_PAD_RGMII_RD3__GPIO6_IO29&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0001B030&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt; color: black;"&gt;==========&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt; color: black;"&gt;usb2553-enctlgpio = &amp;lt;&amp;amp;gpio6 24 0&amp;gt;;&lt;BR /&gt;usbfault-enctlgpio= &amp;lt;&amp;amp;gpio6 29 0&amp;gt;;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt; color: black;"&gt;/**********************************************************/&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 May 2018 10:08:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RGMII-RX-CTL-cannot-output-high-level-signal-when-configured-as/m-p/758310#M117917</guid>
      <dc:creator>hi_shawn</dc:creator>
      <dc:date>2018-05-16T10:08:17Z</dc:date>
    </item>
    <item>
      <title>Re: RGMII_RX_CTL cannot output high level signal when configured as GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RGMII-RX-CTL-cannot-output-high-level-signal-when-configured-as/m-p/758311#M117918</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shawn&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is there some rgmii circuit on the board, as for example on i.MX6QP Sabre SD schematic SPF-28857&lt;BR /&gt;these two signals are connected to outputs of AR8031 (U516) RGMII_RXD3, RGMII_RXDV.&lt;BR /&gt;In general one can attach jtag and check iomux settings and try manually set them to '1' signal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 May 2018 01:12:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RGMII-RX-CTL-cannot-output-high-level-signal-when-configured-as/m-p/758311#M117918</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-05-17T01:12:21Z</dc:date>
    </item>
    <item>
      <title>Re: RGMII_RX_CTL cannot output high level signal when configured as GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RGMII-RX-CTL-cannot-output-high-level-signal-when-configured-as/m-p/758312#M117919</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; background-color: #ffffff;"&gt;Pins RGMII_RX_CTL and&amp;nbsp;&lt;SPAN&gt;RGMII_RD3 don't connect to 8031.&amp;nbsp; I want configure them to ALT5 and ALT5. Please refer to the pictures below. As i mentioned, the pins&amp;nbsp;&lt;SPAN style="background-color: #ffffff;"&gt;GPIO_7 and GPIO_8 are OK. But i cannot find the root cause. Anything else i should care about?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; background-color: #ffffff;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; background-color: #ffffff;"&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/7563i692CEF61A9E9BD0D/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; background-color: #ffffff;"&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/7659i371D8B195EF5A065/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 May 2018 03:32:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RGMII-RX-CTL-cannot-output-high-level-signal-when-configured-as/m-p/758312#M117919</guid>
      <dc:creator>hi_shawn</dc:creator>
      <dc:date>2018-05-18T03:32:42Z</dc:date>
    </item>
    <item>
      <title>Re: RGMII_RX_CTL cannot output high level signal when configured as GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RGMII-RX-CTL-cannot-output-high-level-signal-when-configured-as/m-p/758313#M117920</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shawn&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please attach jtag debugger and try to set outputs of these pads using jtag.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 May 2018 03:36:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RGMII-RX-CTL-cannot-output-high-level-signal-when-configured-as/m-p/758313#M117920</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-05-18T03:36:51Z</dc:date>
    </item>
  </channel>
</rss>