<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: vAnalyzer in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/vAnalyzer/m-p/757472#M117820</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Manoj,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;vAnalyzer is, like all other tools in the VTK, a Windows application, which is a bit unfortunate since most i.MX boards probably run Linux, and hence the developers probably run Linux on their desktop machine as well. Fortunately, it runs fine under Wine, simply running &lt;CODE&gt;wine setup.exe&lt;/CODE&gt; will install vAnalyzer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can see the steps to use vAnalyzer in Linux, which I think you can apply in QNX, which NXP does not support.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.kdab.com/profile-qtquick-applications-mx-6-vanalyzer/" title="https://www.kdab.com/profile-qtquick-applications-mx-6-vanalyzer/"&gt;How to Profile QtQuick applications on Freescale i.MX 6 with vAnalyzer - KDAB&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 01 Dec 2017 18:14:12 GMT</pubDate>
    <dc:creator>jamesbone</dc:creator>
    <dc:date>2017-12-01T18:14:12Z</dc:date>
    <item>
      <title>vAnalyzer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/vAnalyzer/m-p/757471#M117819</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am&amp;nbsp;developing an OpenGL ES 2.0 application in QNX 6.0 OS running on&amp;nbsp;IMX6 Quad+&lt;/P&gt;&lt;P&gt;I&amp;nbsp;wanted to analyze the performance using the vAnalyzer and therefore can someone share the details about how this can be done in the QNX environment?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Dec 2017 12:38:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/vAnalyzer/m-p/757471#M117819</guid>
      <dc:creator>manoje_s_</dc:creator>
      <dc:date>2017-12-01T12:38:19Z</dc:date>
    </item>
    <item>
      <title>Re: vAnalyzer</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/vAnalyzer/m-p/757472#M117820</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Manoj,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;vAnalyzer is, like all other tools in the VTK, a Windows application, which is a bit unfortunate since most i.MX boards probably run Linux, and hence the developers probably run Linux on their desktop machine as well. Fortunately, it runs fine under Wine, simply running &lt;CODE&gt;wine setup.exe&lt;/CODE&gt; will install vAnalyzer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can see the steps to use vAnalyzer in Linux, which I think you can apply in QNX, which NXP does not support.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.kdab.com/profile-qtquick-applications-mx-6-vanalyzer/" title="https://www.kdab.com/profile-qtquick-applications-mx-6-vanalyzer/"&gt;How to Profile QtQuick applications on Freescale i.MX 6 with vAnalyzer - KDAB&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Dec 2017 18:14:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/vAnalyzer/m-p/757472#M117820</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2017-12-01T18:14:12Z</dc:date>
    </item>
  </channel>
</rss>