<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: system wakeup from shutdown</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/system-wakeup-from-shutdown/m-p/756935#M117731</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos, Actually it was not working earlier also but after NXP help they recommended changing a mask value from 0x61 to 0x6b for&amp;nbsp;&lt;/P&gt;&lt;P&gt;snvs_poweroff: snvs-poweroff&amp;nbsp; in imx6ul.dtsi. But now this doesn't work.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Feb 2018 12:08:12 GMT</pubDate>
    <dc:creator>pratyushtomar</dc:creator>
    <dc:date>2018-02-22T12:08:12Z</dc:date>
    <item>
      <title>system wakeup from shutdown</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/system-wakeup-from-shutdown/m-p/756933#M117729</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am i.MX6UL processor and earlier when I was using kernel "Linux imx6ulevk 4.1.15-1.1.1+gd5d7c02" my board used to wakeup from shutdown if I set the /sys/classrtc/rtc0/wakealarm before shutdown with no problems. But after upgrading kernel to "Linux imx6ulevk 4.1.15-1.2.0+g77f6154" my board is not waking up from shutdown even though everything is same as before except for change in kernel. What can be the reason for this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jan 2018 13:03:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/system-wakeup-from-shutdown/m-p/756933#M117729</guid>
      <dc:creator>pratyushtomar</dc:creator>
      <dc:date>2018-01-25T13:03:24Z</dc:date>
    </item>
    <item>
      <title>Re: system wakeup from shutdown</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/system-wakeup-from-shutdown/m-p/756934#M117730</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pratyush,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;most likely the problem is the device tree. The drivers in the newest kernel can be referencing the device tree nodes in a different way than the previous kernel, so you need a device tree that matches with the new kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jan 2018 20:33:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/system-wakeup-from-shutdown/m-p/756934#M117730</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2018-01-25T20:33:42Z</dc:date>
    </item>
    <item>
      <title>Re: system wakeup from shutdown</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/system-wakeup-from-shutdown/m-p/756935#M117731</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos, Actually it was not working earlier also but after NXP help they recommended changing a mask value from 0x61 to 0x6b for&amp;nbsp;&lt;/P&gt;&lt;P&gt;snvs_poweroff: snvs-poweroff&amp;nbsp; in imx6ul.dtsi. But now this doesn't work.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Feb 2018 12:08:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/system-wakeup-from-shutdown/m-p/756935#M117731</guid>
      <dc:creator>pratyushtomar</dc:creator>
      <dc:date>2018-02-22T12:08:12Z</dc:date>
    </item>
  </channel>
</rss>