<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Yocto QA error? File already stripped</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-QA-error-File-already-stripped/m-p/756508#M117679</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have you try to build in a new 'build' folder?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Nov 2017 06:55:47 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2017-11-09T06:55:47Z</dc:date>
    <item>
      <title>Yocto QA error? File already stripped</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-QA-error-File-already-stripped/m-p/756507#M117678</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Following errors I receive when building a basic yocto image (morty). Even when deleting my complete temp-directory and build again. This is just when building the plain core-image-minimal for sabreauto. Does anybody have an idea where this comes from? Everything seems to compile ok, but starts to have problems when do_package.&lt;/P&gt;&lt;P&gt;To be complete, this is on a system where it was working before. But as it was a 32bit system before, I migrated to a 64bit system last week (multiarch). Since then, it stopped working. If possible, I want to fix it on this system.&lt;/P&gt;&lt;P&gt;Anybody has an idea what the issue could be?&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;ERROR: base-files-3.0.14-r89 do_package: QA Issue: File '/etc/skel/.bashrc' from base-files was already stripped, this will prevent future debugging! [already-stripped]&lt;BR /&gt;ERROR: base-files-3.0.14-r89 do_package: QA Issue: File '/etc/skel/.profile' from base-files was already stripped, this will prevent future debugging! [already-stripped]&lt;BR /&gt;ERROR: base-files-3.0.14-r89 do_package: Fatal QA errors found, failing task.&lt;BR /&gt;ERROR: base-files-3.0.14-r89 do_package: Function failed: do_package&lt;BR /&gt;ERROR: Logfile of failure stored in: /opt/yocto/fsl-community-bsp_morty/build-sabre/tmp/work/imx6qsabreauto-fslc-linux-gnueabi/base-files/3.0.14-r89/temp/log.do_package.35314&lt;BR /&gt;ERROR: Task (/opt/yocto/fsl-community-bsp_morty/sources/poky/meta/recipes-core/base-files/base-files_3.0.14.bb:do_package) failed with exit code '1'&lt;BR /&gt;ERROR: glibc-2.24-r0 do_package: QA Issue: File '/etc/nscd.conf' from glibc was already stripped, this will prevent future debugging! [already-stripped]&lt;BR /&gt;ERROR: glibc-2.24-r0 do_package: QA Issue: File '/etc/init.d/nscd' from glibc was already stripped, this will prevent future debugging! [already-stripped]&lt;BR /&gt;ERROR: glibc-2.24-r0 do_package: QA Issue: File '/usr/lib/libpthread.so' from glibc was already stripped, this will prevent future debugging! [already-stripped]&lt;BR /&gt;ERROR: glibc-2.24-r0 do_package: QA Issue: File '/usr/lib/libc.so' from glibc was already stripped, this will prevent future debugging! [already-stripped]&lt;BR /&gt;ERROR: glibc-2.24-r0 do_package: QA Issue: File '/usr/bin/tzselect' from glibc was already stripped, this will prevent future debugging! [already-stripped]&lt;BR /&gt;ERROR: glibc-2.24-r0 do_package: QA Issue: File '/usr/bin/catchsegv' from glibc was already stripped, this will prevent future debugging! [already-stripped]&lt;BR /&gt;ERROR: glibc-2.24-r0 do_package: QA Issue: File '/usr/bin/ldd' from glibc was already stripped, this will prevent future debugging! [already-stripped]&lt;BR /&gt;ERROR: glibc-2.24-r0 do_package: Fatal QA errors found, failing task.&lt;BR /&gt;ERROR: glibc-2.24-r0 do_package: Function failed: do_package&lt;BR /&gt;ERROR: Logfile of failure stored in: /opt/yocto/fsl-community-bsp_morty/build-sabre/tmp/work/armv7at2hf-neon-fslc-linux-gnueabi/glibc/2.24-r0/temp/log.do_package.83637&lt;BR /&gt;ERROR: Task (/opt/yocto/fsl-community-bsp_morty/sources/poky/meta/recipes-core/glibc/glibc_2.24.bb:do_package) failed with exit code '1'&lt;BR /&gt;ERROR: sysvinit-inittab-2.88dsf-r10 do_package: QA Issue: File '/bin/start_getty' from sysvinit-inittab was already stripped, this will prevent future debugging! [already-stripped]&lt;BR /&gt;ERROR: sysvinit-inittab-2.88dsf-r10 do_package: Fatal QA errors found, failing task.&lt;BR /&gt;ERROR: sysvinit-inittab-2.88dsf-r10 do_package: Function failed: do_package&lt;BR /&gt;ERROR: Logfile of failure stored in: /opt/yocto/fsl-community-bsp_morty/build-sabre/tmp/work/imx6qsabreauto-fslc-linux-gnueabi/sysvinit-inittab/2.88dsf-r10/temp/log.do_package.38593&lt;BR /&gt;ERROR: Task (/opt/yocto/fsl-community-bsp_morty/sources/poky/meta/recipes-core/sysvinit/sysvinit-inittab_2.88dsf.bb:do_package) failed with exit code '1'&lt;BR /&gt;ERROR: qemuwrapper-cross-1.0-r0 do_package: QA Issue: File '/usr/bin/crossscripts/qemuwrapper' from qemuwrapper-cross was already stripped, this will prevent future debugging! [already-stripped]&lt;BR /&gt;ERROR: qemuwrapper-cross-1.0-r0 do_package: Fatal QA errors found, failing task.&lt;BR /&gt;ERROR: qemuwrapper-cross-1.0-r0 do_package: Function failed: do_package&lt;BR /&gt;ERROR: Logfile of failure stored in: /opt/yocto/fsl-community-bsp_morty/build-sabre/tmp/work/armv7at2hf-neon-fslc-linux-gnueabi/qemuwrapper-cross/1.0-r0/temp/log.do_package.90399&lt;BR /&gt;ERROR: Task (/opt/yocto/fsl-community-bsp_morty/sources/poky/meta/recipes-devtools/qemu/qemuwrapper-cross_1.0.bb:do_package) failed with exit code '1'&lt;BR /&gt;WARNING: glibc-locale-2.24-r0 do_package_qa: QA Issue: /usr/bin/localedef contained in package localedef requires libc.so.6, but no providers found in RDEPENDS_localedef? [file-rdeps]&lt;BR /&gt;NOTE: Tasks Summary: Attempted 1689 tasks of which 290 didn't need to be rerun and 4 failed.&lt;BR /&gt;NOTE: Writing buildhistory&lt;/P&gt;&lt;P&gt;Summary: 4 tasks failed:&lt;BR /&gt; /opt/yocto/fsl-community-bsp_morty/sources/poky/meta/recipes-core/base-files/base-files_3.0.14.bb:do_package&lt;BR /&gt; /opt/yocto/fsl-community-bsp_morty/sources/poky/meta/recipes-core/glibc/glibc_2.24.bb:do_package&lt;BR /&gt; /opt/yocto/fsl-community-bsp_morty/sources/poky/meta/recipes-core/sysvinit/sysvinit-inittab_2.88dsf.bb:do_package&lt;BR /&gt; /opt/yocto/fsl-community-bsp_morty/sources/poky/meta/recipes-devtools/qemu/qemuwrapper-cross_1.0.bb:do_package&lt;BR /&gt;Summary: There were 2 WARNING messages shown.&lt;BR /&gt;Summary: There were 19 ERROR messages shown, returning a non-zero exit code.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Nov 2017 21:36:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-QA-error-File-already-stripped/m-p/756507#M117678</guid>
      <dc:creator>woutervh</dc:creator>
      <dc:date>2017-11-07T21:36:08Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto QA error? File already stripped</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-QA-error-File-already-stripped/m-p/756508#M117679</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have you try to build in a new 'build' folder?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Nov 2017 06:55:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-QA-error-File-already-stripped/m-p/756508#M117679</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2017-11-09T06:55:47Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto QA error? File already stripped</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-QA-error-File-already-stripped/m-p/756509#M117680</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, but in the meantime, I was able to fix it. What exactly caused it, I don't know. But my machine at that time was a mix of 32bit &amp;amp; 64bit packages.&lt;/P&gt;&lt;P&gt;After updating grep, awk, automake, fileinfo, systemd, etc... to 64-bit, everything works afterwards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Nov 2017 08:14:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-QA-error-File-already-stripped/m-p/756509#M117680</guid>
      <dc:creator>woutervh</dc:creator>
      <dc:date>2017-11-13T08:14:38Z</dc:date>
    </item>
  </channel>
</rss>