<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic About boot from eMMC v5.1 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/About-boot-from-eMMC-v5-1/m-p/756396#M117660</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, everyone:&lt;/P&gt;&lt;P&gt;Our custom imx6 dual lite board using an eMMC v5.1 chip, now I am trying to boot from eMMC(L4.1.15_2.1.0: SPL + u-boot, image, rootfs all write to eMMC). I checked the Reference manual of imx6(IMX6SDLRM.pdf), in the section &amp;lt;8.5.3.1 Expansion device eFUSE configuration&amp;gt;, it described as following:&lt;/P&gt;&lt;P&gt;The boot code supports these standards:&lt;BR /&gt;• MMCv4.4 or less&lt;BR /&gt;• eMMCv4.4 or less&lt;BR /&gt;• SDv2.0 or less&lt;BR /&gt;• eSDv2.10 rev-0.9, with or without FAST_BOOT&lt;BR /&gt;• SDXCv3.0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does this mean imx6 not support eMMC v5.1?&lt;/P&gt;&lt;P&gt;About the kernel eMMC version patch, I already checked, it is updated in L4.1.15.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 02 Apr 2018 09:09:26 GMT</pubDate>
    <dc:creator>westbrook</dc:creator>
    <dc:date>2018-04-02T09:09:26Z</dc:date>
    <item>
      <title>About boot from eMMC v5.1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-boot-from-eMMC-v5-1/m-p/756396#M117660</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, everyone:&lt;/P&gt;&lt;P&gt;Our custom imx6 dual lite board using an eMMC v5.1 chip, now I am trying to boot from eMMC(L4.1.15_2.1.0: SPL + u-boot, image, rootfs all write to eMMC). I checked the Reference manual of imx6(IMX6SDLRM.pdf), in the section &amp;lt;8.5.3.1 Expansion device eFUSE configuration&amp;gt;, it described as following:&lt;/P&gt;&lt;P&gt;The boot code supports these standards:&lt;BR /&gt;• MMCv4.4 or less&lt;BR /&gt;• eMMCv4.4 or less&lt;BR /&gt;• SDv2.0 or less&lt;BR /&gt;• eSDv2.10 rev-0.9, with or without FAST_BOOT&lt;BR /&gt;• SDXCv3.0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does this mean imx6 not support eMMC v5.1?&lt;/P&gt;&lt;P&gt;About the kernel eMMC version patch, I already checked, it is updated in L4.1.15.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Apr 2018 09:09:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-boot-from-eMMC-v5-1/m-p/756396#M117660</guid>
      <dc:creator>westbrook</dc:creator>
      <dc:date>2018-04-02T09:09:26Z</dc:date>
    </item>
    <item>
      <title>Re: About boot from eMMC v5.1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-boot-from-eMMC-v5-1/m-p/756397#M117661</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi xiao&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please look at&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-332187"&gt;EMMC 5.0 and EMMC 5.1 work on i.MX6&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Apr 2018 00:19:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-boot-from-eMMC-v5-1/m-p/756397#M117661</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-04-03T00:19:02Z</dc:date>
    </item>
    <item>
      <title>Re: About boot from eMMC v5.1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-boot-from-eMMC-v5-1/m-p/756398#M117662</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igorpadykov:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your answer, I already checked this eMMC rev issue.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I modified the BOOT_CFG1[4] = 0, which means&amp;nbsp;Normal Boot, previously it is 1. Now I can boot SPL from eMMC. Does eMMC support Fast Boot?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Other important settings:&lt;/P&gt;&lt;P&gt;Boot configuration bytes [PARTITION_CONFIG: 0x49]&lt;BR /&gt; Boot Partition 1 enabled&lt;BR /&gt; R/W Boot Partition 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;xiao&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Apr 2018 01:42:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-boot-from-eMMC-v5-1/m-p/756398#M117662</guid>
      <dc:creator>westbrook</dc:creator>
      <dc:date>2018-04-03T01:42:16Z</dc:date>
    </item>
  </channel>
</rss>