<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: PMIC connection with Linux</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-connection-with-Linux/m-p/755958#M117581</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nemanja&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;linux knows which regulator to use looking at dts file, for example&lt;/P&gt;&lt;P&gt;linux/arch/arm/boot/dts/imx6dl.dtsi file entriy "arm-supply" and others&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/arch/arm/boot/dts/imx6dl.dtsi?h=imx_4.9.11_1.0.0_ga" title="http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/arch/arm/boot/dts/imx6dl.dtsi?h=imx_4.9.11_1.0.0_ga"&gt;linux-imx.git - i.MX Linux Kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also one can look at&amp;nbsp;PFUZE regulator driver sources described in&lt;/P&gt;&lt;P&gt;Chapter PF100 Regulator Driver of Linux Reference Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Nov 2017 23:16:33 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2017-11-07T23:16:33Z</dc:date>
    <item>
      <title>PMIC connection with Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-connection-with-Linux/m-p/755957#M117580</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I am using a board with i.MX6Q processor and LTC3676 PMIC. At the moment I would like to realize how is a PMIC actually connected and instantiated in Linux. I looked at the i.MX6 Linux user manual, and there was explained that the on the top sits the regulator core drive, followed by the PF100-core driver and followed by the PF100 regulator driver (although my current sources have only pfuze100-regulator driver).&lt;/P&gt;&lt;P&gt;I see that regulator core driver has very general commands which internally call API of the actual PMIC. I also see that inside the device tree, it is possible to have a PMIC entry with its child regulators.&lt;/P&gt;&lt;P&gt;What I do not understand at the moment is how Linux knows which regulator is used for SoC core voltage, which one provides VDD_ARM, etc. I belive that when scaling the frequency down, the system should know which voltage can be lowered.&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Nov 2017 15:52:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PMIC-connection-with-Linux/m-p/755957#M117580</guid>
      <dc:creator>nexy_sm</dc:creator>
      <dc:date>2017-11-07T15:52:39Z</dc:date>
    </item>
    <item>
      <title>Re: PMIC connection with Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-connection-with-Linux/m-p/755958#M117581</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nemanja&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;linux knows which regulator to use looking at dts file, for example&lt;/P&gt;&lt;P&gt;linux/arch/arm/boot/dts/imx6dl.dtsi file entriy "arm-supply" and others&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/arch/arm/boot/dts/imx6dl.dtsi?h=imx_4.9.11_1.0.0_ga" title="http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/arch/arm/boot/dts/imx6dl.dtsi?h=imx_4.9.11_1.0.0_ga"&gt;linux-imx.git - i.MX Linux Kernel&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also one can look at&amp;nbsp;PFUZE regulator driver sources described in&lt;/P&gt;&lt;P&gt;Chapter PF100 Regulator Driver of Linux Reference Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Nov 2017 23:16:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PMIC-connection-with-Linux/m-p/755958#M117581</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-11-07T23:16:33Z</dc:date>
    </item>
  </channel>
</rss>