<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.mx6 Single SSI Port for Two usersapce Application and PCM Data loop back in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Single-SSI-Port-for-Two-usersapce-Application-and-PCM-Data/m-p/754939#M117460</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;igorpadykov,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the information. According to the IMX6DQRM Datasheet, The SSI Provides&amp;nbsp;2 sets of Transmit and Receive FIFOs. Each of the four FIFOs is 15x32 bits. The two sets of Tx/Rx FIFOs can be used in Network mode to provide 2 independent channels for transmission and reception. But, It has only one Transmit Shift Register (TXSR) and Receive Shift Register.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Will SSI take care of two application date&amp;nbsp;simultaneously in network mode?&lt;/P&gt;&lt;P&gt;Is there any example of network mode with i.MX6 SSI?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Nov 2017 04:20:08 GMT</pubDate>
    <dc:creator>jegathesanshanm</dc:creator>
    <dc:date>2017-11-08T04:20:08Z</dc:date>
    <item>
      <title>i.mx6 Single SSI Port for Two usersapce Application and PCM Data loop back</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Single-SSI-Port-for-Two-usersapce-Application-and-PCM-Data/m-p/754937#M117458</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#IMX6DQRM has three #SSI Interface. I want to use only one of the SSI port(i.e SSI3) for two userspace #Alsa application in loopback mode, As shown in Figure.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="IMX6_SSI.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21272i8CDF179AE8EC9442/image-size/large?v=v2&amp;amp;px=999" role="button" title="IMX6_SSI.png" alt="IMX6_SSI.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to route the data using SSI Network mode?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Note:&lt;/STRONG&gt; I'm trying use only one AUDMUX Internal port(PORT 7) for loopback.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any comments or suggestions are highly appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;cheers,&lt;/P&gt;&lt;P&gt;Jegathesan S&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Nov 2017 15:18:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Single-SSI-Port-for-Two-usersapce-Application-and-PCM-Data/m-p/754937#M117458</guid>
      <dc:creator>jegathesanshanm</dc:creator>
      <dc:date>2017-11-07T15:18:07Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6 Single SSI Port for Two usersapce Application and PCM Data loop back</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Single-SSI-Port-for-Two-usersapce-Application-and-PCM-Data/m-p/754938#M117459</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jegathesan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am afraid full loopback is not possible as SSI-AUDMUX connection&lt;/P&gt;&lt;P&gt;has one receive and one transmit data, as for example depicted on&lt;/P&gt;&lt;P&gt;AN2628 Programming Audio Applications, Figure 1 SSI and AUDMUX Port Arrangements&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN2628.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN2628.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Nov 2017 23:04:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Single-SSI-Port-for-Two-usersapce-Application-and-PCM-Data/m-p/754938#M117459</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-11-07T23:04:31Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6 Single SSI Port for Two usersapce Application and PCM Data loop back</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Single-SSI-Port-for-Two-usersapce-Application-and-PCM-Data/m-p/754939#M117460</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;igorpadykov,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the information. According to the IMX6DQRM Datasheet, The SSI Provides&amp;nbsp;2 sets of Transmit and Receive FIFOs. Each of the four FIFOs is 15x32 bits. The two sets of Tx/Rx FIFOs can be used in Network mode to provide 2 independent channels for transmission and reception. But, It has only one Transmit Shift Register (TXSR) and Receive Shift Register.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Will SSI take care of two application date&amp;nbsp;simultaneously in network mode?&lt;/P&gt;&lt;P&gt;Is there any example of network mode with i.MX6 SSI?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Nov 2017 04:20:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Single-SSI-Port-for-Two-usersapce-Application-and-PCM-Data/m-p/754939#M117460</guid>
      <dc:creator>jegathesanshanm</dc:creator>
      <dc:date>2017-11-08T04:20:08Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6 Single SSI Port for Two usersapce Application and PCM Data loop back</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Single-SSI-Port-for-Two-usersapce-Application-and-PCM-Data/m-p/754940#M117461</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jegathesan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not aware of network example. Yes there are 2 sets of Transmit and Receive FIFOs&lt;/P&gt;&lt;P&gt;but only one receive and one transmit data as depicted on Figure 61-1.&lt;/P&gt;&lt;P&gt;SSI Block Diagram i.MX6DQ Reference Manual.&lt;/P&gt;&lt;P&gt;Description of operation is provided in sect.61.9.1 SSI Transmit Data Register n (SSIx_STXn) :&lt;BR /&gt;If both FIFOs are in use, data is alternately transferred from STX0 and STX1, to TXSR.&lt;BR /&gt;Data written to these registers is transferred to the Transmit Shift Register (TXSR)..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Nov 2017 07:35:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-Single-SSI-Port-for-Two-usersapce-Application-and-PCM-Data/m-p/754940#M117461</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-11-08T07:35:53Z</dc:date>
    </item>
  </channel>
</rss>