<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Getting a 4K HDMI output on MCIMX8M-EVK</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Getting-a-4K-HDMI-output-on-MCIMX8M-EVK/m-p/754672#M117413</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please tell the exact part number of your board? I tested with the same image and the same bootargs (I used the last option of your bootargs) that you used, and it worked on my board. Furthermore, it also can be the display that you are using.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Feb 2018 21:01:38 GMT</pubDate>
    <dc:creator>diegoadrian</dc:creator>
    <dc:date>2018-02-22T21:01:38Z</dc:date>
    <item>
      <title>Getting a 4K HDMI output on MCIMX8M-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Getting-a-4K-HDMI-output-on-MCIMX8M-EVK/m-p/754669#M117410</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was trying to get 4K hdmi output working with linux but I could not get it to work. ( 1920 x 1080 works fine )&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;For 1080p I used this for u-boot which works.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;setenv mmcargs 'setenv bootargs console=${console} root=${mmcroot} video=HDMI-A-1:1920x1080-32@60'&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&lt;/P&gt;&lt;P&gt;I am using NXP i.MX Release Distro 4.9.51-mx8-beta&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have tried a few different options to get 4K to work but none work&lt;/P&gt;&lt;P&gt;setenv mmcargs 'setenv bootargs console=${console} root=${mmcroot} video=HDMI-A-1:3840x2160-32@60'&lt;BR /&gt;setenv mmcargs 'setenv bootargs console=${console} root=${mmcroot} video=HDMI-A-1:4096x2160-32@60'&lt;/P&gt;&lt;P&gt;setenv mmcargs 'setenv bootargs console=${console} root=${mmcroot} video=HDMI-A-1:3840x2160-32@30'&lt;BR /&gt;setenv mmcargs 'setenv bootargs console=${console} root=${mmcroot} video=HDMI-A-1:3840x2160-32@25'&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using MCIMX8M-EVK part number 700-29615 REV A&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 17 Feb 2018 13:29:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Getting-a-4K-HDMI-output-on-MCIMX8M-EVK/m-p/754669#M117410</guid>
      <dc:creator>louisryan</dc:creator>
      <dc:date>2018-02-17T13:29:53Z</dc:date>
    </item>
    <item>
      <title>Re: Getting a 4K HDMI output on MCIMX8M-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Getting-a-4K-HDMI-output-on-MCIMX8M-EVK/m-p/754670#M117411</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you tried with the default bootargs? The default Bootargs that the image has, are for 4K video output.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Feb 2018 18:38:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Getting-a-4K-HDMI-output-on-MCIMX8M-EVK/m-p/754670#M117411</guid>
      <dc:creator>diegoadrian</dc:creator>
      <dc:date>2018-02-20T18:38:53Z</dc:date>
    </item>
    <item>
      <title>Re: Getting a 4K HDMI output on MCIMX8M-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Getting-a-4K-HDMI-output-on-MCIMX8M-EVK/m-p/754671#M117412</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Diego,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"Have you tried with the default bootargs? The default Bootargs that the image has, are for 4K video output"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use this image : fsl-image-qt5-validation-imx-xwayland-imx8mqevk.sdcard ( prebuild binary from nxp )&lt;/P&gt;&lt;P&gt;I copy to SD Card:&amp;nbsp; sudo dd if=fsl-image-qt5-validation-imx-xwayland-imx8mqevk.sdcard of=/dev/sdf bs=1M &amp;amp;&amp;amp; sync&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I apply power to the board I get the linux boot process&amp;nbsp; via the debug uart. But there is no HDMI output. See the u-boot printenv output below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;"For 1080p I used this for u-boot which works.&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;setenv mmcargs 'setenv bootargs console=${console} root=${mmcroot} video=HDMI-A-1:1920x1080-32@60'"&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;But I want it to work for 4K. What do you think I should change?&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;Thanks&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;Louis&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;U-BOOT - Printenv&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;----------------------------------------------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;U-Boot SPL 2017.03-imx_v2017.03_4.9.51_imx8m_beta+g0adb492 (Dec 22 2017 - 04:21:08)&lt;BR /&gt;PMIC: PFUZE100 ID=0x10&lt;BR /&gt;check ddr4_pmu_train_imem code&lt;BR /&gt;check ddr4_pmu_train_imem code pass&lt;BR /&gt;check ddr4_pmu_train_dmem code&lt;BR /&gt;check ddr4_pmu_train_dmem code pass&lt;BR /&gt;PLL bypass to 100MTS setting done&lt;BR /&gt;Training PASS&lt;BR /&gt;PLL bypass to 400MTS setting done&lt;BR /&gt;Training PASS&lt;BR /&gt;Training PASS&lt;BR /&gt;check ddr4_pmu_train_imem code&lt;BR /&gt;check ddr4_pmu_train_imem code pass&lt;BR /&gt;check ddr4_pmu_train_dmem code&lt;BR /&gt;check ddr4_pmu_train_dmem code pass&lt;BR /&gt;Training PASS&lt;BR /&gt;Normal Boot&lt;BR /&gt;Trying to boot from MMC2&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot 2017.03-imx_v2017.03_4.9.51_imx8m_beta+g0adb492 (Dec 22 2017 - 04:21:08 +0800)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX8MQ rev2.0 1500 MHz (running at 1000 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 38C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: Freescale i.MX8MQ EVK&lt;BR /&gt;DRAM: 3 GiB&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;*** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1 is current device&lt;BR /&gt;Net:&lt;BR /&gt;Warning: ethernet@30be0000 using MAC address from ROM&lt;BR /&gt;eth0: ethernet@30be0000&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;u-boot=&amp;gt; printenv&lt;BR /&gt;baudrate=115200&lt;BR /&gt;boot_fdt=try&lt;BR /&gt;bootcmd=mmc dev ${mmcdev}; if mmc rescan; then if run loadbootscript; then run bootscript; else if run loadimage; then run mmcboot; else run netboot; fi; fi; else booti ${loadaddr} - ${fdt_addr}; fi&lt;BR /&gt;bootcmd_mfg=run mfgtool_args;booti ${loadaddr} ${initrd_addr} ${fdt_addr};&lt;BR /&gt;bootdelay=2&lt;BR /&gt;bootscript=echo Running bootscript from mmc ...; source&lt;BR /&gt;console=ttymxc0,115200 earlycon=ec_imx6q,0x30860000,115200&lt;BR /&gt;ethaddr=00:04:9f:05:68:f1&lt;BR /&gt;ethprime=FEC&lt;BR /&gt;fdt_addr=0x43000000&lt;BR /&gt;fdt_file=fsl-imx8mq-evk.dtb&lt;BR /&gt;fdt_high=0xffffffffffffffff&lt;BR /&gt;fdtcontroladdr=ff91dc48&lt;BR /&gt;image=Image&lt;BR /&gt;initrd_addr=0x43800000&lt;BR /&gt;initrd_high=0xffffffffffffffff&lt;BR /&gt;loadaddr=0x40480000&lt;BR /&gt;loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};&lt;BR /&gt;loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}&lt;BR /&gt;loadimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${image}&lt;BR /&gt;mfgtool_args=setenv bootargs console=${console},${baudrate} rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber="" clk_ignore_unused&lt;BR /&gt;mmcargs=setenv bootargs console=${console} root=${mmcroot}&lt;BR /&gt;mmcautodetect=yes&lt;BR /&gt;mmcboot=echo Booting from mmc ...; run mmcargs; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then booti ${loadaddr} - ${fdt_addr}; else echo WARN: Cannot load the DT; fi; else echo wait for boot; fi;&lt;BR /&gt;mmcdev=1&lt;BR /&gt;mmcpart=1&lt;BR /&gt;mmcroot=/dev/mmcblk1p2 rootwait rw&lt;BR /&gt;netargs=setenv bootargs console=${console} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp&lt;BR /&gt;netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${loadaddr} ${image}; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if ${get_cmd} ${fdt_addr} ${fdt_file}; then booti ${loadaddr} - ${fdt_addr}; else echo WARN: Cannot load the DT; fi; else booti; fi;&lt;BR /&gt;script=boot.scr&lt;BR /&gt;stderr=serial&lt;BR /&gt;stdin=serial&lt;BR /&gt;stdout=serial&lt;/P&gt;&lt;P&gt;Environment size: 2036/4092 bytes&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Feb 2018 16:06:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Getting-a-4K-HDMI-output-on-MCIMX8M-EVK/m-p/754671#M117412</guid>
      <dc:creator>louisryan</dc:creator>
      <dc:date>2018-02-21T16:06:18Z</dc:date>
    </item>
    <item>
      <title>Re: Getting a 4K HDMI output on MCIMX8M-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Getting-a-4K-HDMI-output-on-MCIMX8M-EVK/m-p/754672#M117413</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please tell the exact part number of your board? I tested with the same image and the same bootargs (I used the last option of your bootargs) that you used, and it worked on my board. Furthermore, it also can be the display that you are using.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Feb 2018 21:01:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Getting-a-4K-HDMI-output-on-MCIMX8M-EVK/m-p/754672#M117413</guid>
      <dc:creator>diegoadrian</dc:creator>
      <dc:date>2018-02-22T21:01:38Z</dc:date>
    </item>
    <item>
      <title>Re: Getting a 4K HDMI output on MCIMX8M-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Getting-a-4K-HDMI-output-on-MCIMX8M-EVK/m-p/754673#M117414</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Diego,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using MCIMX8M-EVK part number 700-29615 REV A - SCH-29615 REV B3&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I use the last option&lt;/P&gt;&lt;P&gt;"setenv mmcargs 'setenv bootargs console=${console} root=${mmcroot} video=HDMI-A-1:3840x2160-32@25'"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I get&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;[&amp;nbsp;&amp;nbsp; 13.679888] [drm:imx_hdp_bridge_mode_set] *ERROR* Unsupport video mode now, 3840x2160, clk=278781&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 14.355477] [drm:imx_hdp_bridge_mode_set] *ERROR* Unsupport video mode now, 3840x2160, clk=278781&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;when I use &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;setenv mmcargs 'setenv bootargs console=${console} root=${mmcroot} video=HDMI-A-1:3840x2160-32@60'&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I get &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;[ 102.219377] VIC 3, pixel clock 594000 kHz&lt;BR /&gt;[ 102.223681] Pixel clock frequency: 594000 kHz, character clock frequency: 594000, color depth is 8-bit.&lt;BR /&gt;[ 102.233272] VCO frequency is 5940000 kHz&lt;BR /&gt;[ 102.239841] CDN_API_General_Write_Register_blocking LANES_CONFIG ret = 0&lt;BR /&gt;[ 102.455079] [drm] HDMI/DP Cable Plug In&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is no error but I get no output.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The monitor I am using does support 3840x2160 and I have tested this. Do you have the make and model of the monitor you are using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Louis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Feb 2018 08:38:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Getting-a-4K-HDMI-output-on-MCIMX8M-EVK/m-p/754673#M117414</guid>
      <dc:creator>louisryan</dc:creator>
      <dc:date>2018-02-26T08:38:44Z</dc:date>
    </item>
    <item>
      <title>Re: Getting a 4K HDMI output on MCIMX8M-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Getting-a-4K-HDMI-output-on-MCIMX8M-EVK/m-p/754674#M117415</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the TLC 49S405 4K TV screen. Furthermore, I did not see the kernel boot up sequence. However, when the GUI started, I could see the image of the Yocto menu.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Furthermore, wich power source are you using? Are you only powering the board with the type c connector?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Feb 2018 15:02:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Getting-a-4K-HDMI-output-on-MCIMX8M-EVK/m-p/754674#M117415</guid>
      <dc:creator>diegoadrian</dc:creator>
      <dc:date>2018-02-26T15:02:19Z</dc:date>
    </item>
    <item>
      <title>Re: Getting a 4K HDMI output on MCIMX8M-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Getting-a-4K-HDMI-output-on-MCIMX8M-EVK/m-p/754675#M117416</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Diego,&lt;/P&gt;&lt;P&gt;I am using the PSU that was supplies with the board.&lt;/P&gt;&lt;P&gt;I am out of the office for a few days. I will do some more testing when \i get back.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,Louis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Feb 2018 07:27:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Getting-a-4K-HDMI-output-on-MCIMX8M-EVK/m-p/754675#M117416</guid>
      <dc:creator>louisryan</dc:creator>
      <dc:date>2018-02-28T07:27:04Z</dc:date>
    </item>
  </channel>
</rss>