<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to do late initialization of LCD driver in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-do-late-initialization-of-LCD-driver/m-p/754390#M117372</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have imx6ul development board with Linux 4.15 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have implemented a splash windows through u-boot, and want to make kernel LCD driver initialization as later as possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The current LCD driver is initialized through:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;__initcall_mxsfb_driver_init6&lt;/P&gt;&lt;P&gt;Is there a way to call this function through Use Space (Application)? If not, how to implement late initialization?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;David Zhou&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Feb 2018 20:32:37 GMT</pubDate>
    <dc:creator>davidzhou</dc:creator>
    <dc:date>2018-02-16T20:32:37Z</dc:date>
    <item>
      <title>How to do late initialization of LCD driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-do-late-initialization-of-LCD-driver/m-p/754390#M117372</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have imx6ul development board with Linux 4.15 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have implemented a splash windows through u-boot, and want to make kernel LCD driver initialization as later as possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The current LCD driver is initialized through:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;__initcall_mxsfb_driver_init6&lt;/P&gt;&lt;P&gt;Is there a way to call this function through Use Space (Application)? If not, how to implement late initialization?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;David Zhou&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Feb 2018 20:32:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-do-late-initialization-of-LCD-driver/m-p/754390#M117372</guid>
      <dc:creator>davidzhou</dc:creator>
      <dc:date>2018-02-16T20:32:37Z</dc:date>
    </item>
    <item>
      <title>Re: How to do late initialization of LCD driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-do-late-initialization-of-LCD-driver/m-p/754391#M117373</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am afraid it is currently not supported and developing custom codes&lt;/P&gt;&lt;P&gt;may be required, probably as example one can look on implementation of&lt;/P&gt;&lt;P&gt;echo 0 &amp;gt; /sys/class/graphics/fb0/blank on&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/323250"&gt;How do I prevent the LCD from turning off after 20 min ?&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 18 Feb 2018 22:43:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-do-late-initialization-of-LCD-driver/m-p/754391#M117373</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-02-18T22:43:27Z</dc:date>
    </item>
  </channel>
</rss>