<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックiMX6Q Pinning Parallel Camera 12-bit</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-Pinning-Parallel-Camera-12-bit/m-p/753919#M117316</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm trying to interface two cameras (Bayer12) via parallel sensor interface. In datasheet of iMX6Q on table 64 I can only find which IPU ports i should use for a 16-bit camera. Which IPU-Ports should I use for 12-bit camera?&lt;BR /&gt;&lt;BR /&gt;Thanks&lt;BR /&gt;Michael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Jun 2018 05:17:46 GMT</pubDate>
    <dc:creator>michael_irsfeld</dc:creator>
    <dc:date>2018-06-06T05:17:46Z</dc:date>
    <item>
      <title>iMX6Q Pinning Parallel Camera 12-bit</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-Pinning-Parallel-Camera-12-bit/m-p/753919#M117316</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm trying to interface two cameras (Bayer12) via parallel sensor interface. In datasheet of iMX6Q on table 64 I can only find which IPU ports i should use for a 16-bit camera. Which IPU-Ports should I use for 12-bit camera?&lt;BR /&gt;&lt;BR /&gt;Thanks&lt;BR /&gt;Michael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jun 2018 05:17:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-Pinning-Parallel-Camera-12-bit/m-p/753919#M117316</guid>
      <dc:creator>michael_irsfeld</dc:creator>
      <dc:date>2018-06-06T05:17:46Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6Q Pinning Parallel Camera 12-bit</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-Pinning-Parallel-Camera-12-bit/m-p/753920#M117317</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi michael,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Verdana','sans-serif';"&gt;For possible sensor connections, please look at the datasheet(s),&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Verdana','sans-serif';"&gt;for example - Table (Camera Input Signal Cross Reference, Format, and Bits Per Cycle) &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Verdana','sans-serif';"&gt;of IMX6DQCEC. &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Verdana','sans-serif';"&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf" title="https://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf"&gt;https://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf&lt;/A&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Verdana','sans-serif';"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Verdana','sans-serif';"&gt;IPU0-1 can be used for 12bit.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jun 2018 16:51:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6Q-Pinning-Parallel-Camera-12-bit/m-p/753920#M117317</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2018-06-06T16:51:19Z</dc:date>
    </item>
  </channel>
</rss>