<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX6 GPIO pull up</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-GPIO-pull-up/m-p/753907#M117307</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Diego,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the answer.&lt;/P&gt;&lt;P&gt;I also think it is strange. I asked customer why pullup/down is required in output mode, but no answer, yet.&lt;/P&gt;&lt;P&gt;Anyway, I understand pullup/down&amp;nbsp; and keeper can enable regardless input and output mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Sugiyama&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 01 Dec 2017 04:45:41 GMT</pubDate>
    <dc:creator>sugiyamatoshihi</dc:creator>
    <dc:date>2017-12-01T04:45:41Z</dc:date>
    <item>
      <title>i.MX6 GPIO pull up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-GPIO-pull-up/m-p/753905#M117305</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question pin output setting.&lt;/P&gt;&lt;P&gt;When a port is&amp;nbsp; output mode, it means OBE is enabled or functional output, is it possible to enable keeper or pull up/down resistor?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In application note, AN5078, there is a description below.&lt;/P&gt;&lt;P&gt;The keeper device is able to keep the previous output value when the output driver is disabled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Sugiyama&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Nov 2017 10:44:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-GPIO-pull-up/m-p/753905#M117305</guid>
      <dc:creator>sugiyamatoshihi</dc:creator>
      <dc:date>2017-11-07T10:44:18Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 GPIO pull up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-GPIO-pull-up/m-p/753906#M117306</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I apologize, but I do not understand what you want to your question.&amp;nbsp; However, if you want to know if it is possible to enable/disable the keeper. Yes, it is possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Nov 2017 21:01:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-GPIO-pull-up/m-p/753906#M117306</guid>
      <dc:creator>diegoadrian</dc:creator>
      <dc:date>2017-11-30T21:01:43Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 GPIO pull up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-GPIO-pull-up/m-p/753907#M117307</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Diego,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the answer.&lt;/P&gt;&lt;P&gt;I also think it is strange. I asked customer why pullup/down is required in output mode, but no answer, yet.&lt;/P&gt;&lt;P&gt;Anyway, I understand pullup/down&amp;nbsp; and keeper can enable regardless input and output mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Sugiyama&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Dec 2017 04:45:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-GPIO-pull-up/m-p/753907#M117307</guid>
      <dc:creator>sugiyamatoshihi</dc:creator>
      <dc:date>2017-12-01T04:45:41Z</dc:date>
    </item>
  </channel>
</rss>