<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックBoot Animation taking too long on iMX6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Boot-Animation-taking-too-long-on-iMX6/m-p/753792#M117301</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using i.MX 6Quad SABRE-AI with Andriod N.&lt;/P&gt;&lt;P&gt;The boot animation log is as follows, but it is taking 42 seconds to boot. Is there a way I can shorten the time? Is there a problem in the log? Also, how to change the permissions?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;init: Starting service 'bootanim'...&lt;BR /&gt;type=1400 audit(12.610:14): avc: denied { getattr } for pid=299 comm="bootanimation1&lt;BR /&gt;type=1400 audit(14.520:15): avc: denied { write } for pid=377 comm="BootAnimation" 1&lt;BR /&gt;type=1400 audit(14.540:16): avc: denied { open } for pid=377 comm="BootAnimation" p1&lt;BR /&gt;capability: warning: `main' uses 32-bit capabilities (legacy support in use)&lt;BR /&gt;period 0 ,timeout is 0, wake up is : 0&lt;BR /&gt;period 0 ,timeout is 0, wake up is : 0&lt;BR /&gt;acc_open&lt;BR /&gt;acc_release&lt;BR /&gt;fec 2188000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr)&lt;BR /&gt;IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready&lt;BR /&gt;period 66 ,timeout is 0, wake up is : 0&lt;BR /&gt;mma enable setting active&lt;BR /&gt;init: Service 'bootanim' (pid 299) exited with status 0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Suhas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 01 Dec 2017 05:56:18 GMT</pubDate>
    <dc:creator>suhaskaundinya</dc:creator>
    <dc:date>2017-12-01T05:56:18Z</dc:date>
    <item>
      <title>Boot Animation taking too long on iMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-Animation-taking-too-long-on-iMX6/m-p/753792#M117301</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using i.MX 6Quad SABRE-AI with Andriod N.&lt;/P&gt;&lt;P&gt;The boot animation log is as follows, but it is taking 42 seconds to boot. Is there a way I can shorten the time? Is there a problem in the log? Also, how to change the permissions?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;init: Starting service 'bootanim'...&lt;BR /&gt;type=1400 audit(12.610:14): avc: denied { getattr } for pid=299 comm="bootanimation1&lt;BR /&gt;type=1400 audit(14.520:15): avc: denied { write } for pid=377 comm="BootAnimation" 1&lt;BR /&gt;type=1400 audit(14.540:16): avc: denied { open } for pid=377 comm="BootAnimation" p1&lt;BR /&gt;capability: warning: `main' uses 32-bit capabilities (legacy support in use)&lt;BR /&gt;period 0 ,timeout is 0, wake up is : 0&lt;BR /&gt;period 0 ,timeout is 0, wake up is : 0&lt;BR /&gt;acc_open&lt;BR /&gt;acc_release&lt;BR /&gt;fec 2188000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr)&lt;BR /&gt;IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready&lt;BR /&gt;period 66 ,timeout is 0, wake up is : 0&lt;BR /&gt;mma enable setting active&lt;BR /&gt;init: Service 'bootanim' (pid 299) exited with status 0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Suhas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Dec 2017 05:56:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-Animation-taking-too-long-on-iMX6/m-p/753792#M117301</guid>
      <dc:creator>suhaskaundinya</dc:creator>
      <dc:date>2017-12-01T05:56:18Z</dc:date>
    </item>
    <item>
      <title>Re: Boot Animation taking too long on iMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-Animation-taking-too-long-on-iMX6/m-p/753793#M117302</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Suhas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, you can optimize the booting process. You can make it by re-arranging the booting process and eliminating some &lt;SPAN class="" lang="en"&gt;&lt;SPAN class=""&gt;unnecessary&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;process for the booting. Unfortunately, we only have implemented this process for Android KitKat. However, you can go with NXP professional service support and they can help you make a patch for Android Nougat.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/support/support/nxp-professional-services:PROFESSIONAL-SERVICE" title="https://www.nxp.com/support/support/nxp-professional-services:PROFESSIONAL-SERVICE"&gt;NXP Professional Services|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Furthermore, this is our patch for Android KitKat, if you are willing to check it out.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-173487"&gt;https://community.nxp.com/docs/DOC-173487&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Dec 2017 17:10:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-Animation-taking-too-long-on-iMX6/m-p/753793#M117302</guid>
      <dc:creator>diegoadrian</dc:creator>
      <dc:date>2017-12-05T17:10:18Z</dc:date>
    </item>
  </channel>
</rss>