<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックArduino interface on MIMXRT1050-EVK</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Arduino-interface-on-MIMXRT1050-EVK/m-p/753476#M117271</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Since the Arduino Interface on the&amp;nbsp;MIMXRT1050-EVK is not populated I would like to know what do I need to integrate mzself the hardware on the board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will for sure need the Arduinio stackable header but the question is if I need anz other hardware component to be solded on the board. As I have seen on the schematics there are some 0 Ohm resistors with the label DNP (Do not place) on some of the pins of the header. Do I need to sold them in case I integrate the Arduino Interface?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 Jan 2018 20:59:24 GMT</pubDate>
    <dc:creator>nebulant</dc:creator>
    <dc:date>2018-01-01T20:59:24Z</dc:date>
    <item>
      <title>Arduino interface on MIMXRT1050-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Arduino-interface-on-MIMXRT1050-EVK/m-p/753476#M117271</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Since the Arduino Interface on the&amp;nbsp;MIMXRT1050-EVK is not populated I would like to know what do I need to integrate mzself the hardware on the board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will for sure need the Arduinio stackable header but the question is if I need anz other hardware component to be solded on the board. As I have seen on the schematics there are some 0 Ohm resistors with the label DNP (Do not place) on some of the pins of the header. Do I need to sold them in case I integrate the Arduino Interface?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Jan 2018 20:59:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Arduino-interface-on-MIMXRT1050-EVK/m-p/753476#M117271</guid>
      <dc:creator>nebulant</dc:creator>
      <dc:date>2018-01-01T20:59:24Z</dc:date>
    </item>
    <item>
      <title>Re: Arduino interface on MIMXRT1050-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Arduino-interface-on-MIMXRT1050-EVK/m-p/753477#M117272</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You just need the Arduino stack header.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jan 2018 17:11:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Arduino-interface-on-MIMXRT1050-EVK/m-p/753477#M117272</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2018-01-04T17:11:15Z</dc:date>
    </item>
    <item>
      <title>Re: Arduino interface on MIMXRT1050-EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Arduino-interface-on-MIMXRT1050-EVK/m-p/753478#M117273</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your answer. I will consider then buying this evaluation board and I'll give here a feedback as soon as I test it. Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jan 2018 11:45:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Arduino-interface-on-MIMXRT1050-EVK/m-p/753478#M117273</guid>
      <dc:creator>nebulant</dc:creator>
      <dc:date>2018-01-17T11:45:45Z</dc:date>
    </item>
  </channel>
</rss>