<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Using MFG tool to write JFFS2 type rootfs in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-MFG-tool-to-write-JFFS2-type-rootfs/m-p/205244#M11720</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using i.MX53 SABRE SMD tablet.&lt;/P&gt;&lt;P&gt;We have used Freescale provided MFG tool to programme the Linux images, like u-boot, uImage, and rootfs.tar.bz2 to the eMMC4.4 card which is of size 4GB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MFG tool internally uses a script file in which it is basically creating a partitions using "dd" command and untar'ing the rootfs.tar.bz2 image in that partition.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But our requirement is to go for JFFS2 type rootfs. &amp;nbsp;&lt;/P&gt;&lt;P&gt;I am not able to understand how it can be worked with MFG tool to flash JFFS2 type rootfs image.&lt;/P&gt;&lt;P&gt;Can anybody give suggestions over this ?&lt;/P&gt;&lt;P&gt;Is it possible to flash JFFS2 rootfs images in i.MX53 SMD tablet board ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks in advance,&lt;/P&gt;&lt;P&gt;-Nagesh A&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Jan 2012 18:24:10 GMT</pubDate>
    <dc:creator>nagesha71</dc:creator>
    <dc:date>2012-01-24T18:24:10Z</dc:date>
    <item>
      <title>Using MFG tool to write JFFS2 type rootfs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-MFG-tool-to-write-JFFS2-type-rootfs/m-p/205244#M11720</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using i.MX53 SABRE SMD tablet.&lt;/P&gt;&lt;P&gt;We have used Freescale provided MFG tool to programme the Linux images, like u-boot, uImage, and rootfs.tar.bz2 to the eMMC4.4 card which is of size 4GB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MFG tool internally uses a script file in which it is basically creating a partitions using "dd" command and untar'ing the rootfs.tar.bz2 image in that partition.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But our requirement is to go for JFFS2 type rootfs. &amp;nbsp;&lt;/P&gt;&lt;P&gt;I am not able to understand how it can be worked with MFG tool to flash JFFS2 type rootfs image.&lt;/P&gt;&lt;P&gt;Can anybody give suggestions over this ?&lt;/P&gt;&lt;P&gt;Is it possible to flash JFFS2 rootfs images in i.MX53 SMD tablet board ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks in advance,&lt;/P&gt;&lt;P&gt;-Nagesh A&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jan 2012 18:24:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-MFG-tool-to-write-JFFS2-type-rootfs/m-p/205244#M11720</guid>
      <dc:creator>nagesha71</dc:creator>
      <dc:date>2012-01-24T18:24:10Z</dc:date>
    </item>
  </channel>
</rss>