<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: USB not recognized on iMX6Q</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-not-recognized-on-iMX6Q/m-p/752785#M117177</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ritesh,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to inform you that MFG Tool it is only supported by Windows 7 .&amp;nbsp; If you are having problems detecting the USB can be related to the Windows HOST, we have seen this error before in Windows 8 and Windows 10 since the tool it is not supported because the driver it is not Certified by windows.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Merry Christmas and Happy new Year.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Dec 2017 20:10:03 GMT</pubDate>
    <dc:creator>jamesbone</dc:creator>
    <dc:date>2017-12-28T20:10:03Z</dc:date>
    <item>
      <title>USB not recognized on iMX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-not-recognized-on-iMX6Q/m-p/752784#M117176</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have designed Hardware around iMX6Q processor for my project.&lt;/P&gt;&lt;P&gt;I have tested all power rails on the processor and it is successfully up. Now I am trying to connect iMX6 (by setting Boot mode as Serial download&amp;nbsp;mode) USB&amp;nbsp;OTG port with PC USB port to download the U-boot binary.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am checking the USB device detection in an MFG tool2.exe from NXP. But It gives me error as "USB not recognized on screen".&lt;/P&gt;&lt;P&gt;I checked in PC device manager and it shows "Unknown USB device (Device Descriptor Request Failed).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would greatly appreciate an early response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Ritesh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Dec 2017 16:01:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-not-recognized-on-iMX6Q/m-p/752784#M117176</guid>
      <dc:creator>riteshpatel</dc:creator>
      <dc:date>2017-12-28T16:01:48Z</dc:date>
    </item>
    <item>
      <title>Re: USB not recognized on iMX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-not-recognized-on-iMX6Q/m-p/752785#M117177</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ritesh,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to inform you that MFG Tool it is only supported by Windows 7 .&amp;nbsp; If you are having problems detecting the USB can be related to the Windows HOST, we have seen this error before in Windows 8 and Windows 10 since the tool it is not supported because the driver it is not Certified by windows.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Merry Christmas and Happy new Year.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Dec 2017 20:10:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-not-recognized-on-iMX6Q/m-p/752785#M117177</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2017-12-28T20:10:03Z</dc:date>
    </item>
    <item>
      <title>Re: USB not recognized on iMX6Q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-not-recognized-on-iMX6Q/m-p/752786#M117178</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi James&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the quick response.&lt;/P&gt;&lt;P&gt;I have checked my Hardware on Windows 7 and iMX6Q USB OTG port detected as a device properly.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Happy New Year.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Dec 2017 06:50:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-not-recognized-on-iMX6Q/m-p/752786#M117178</guid>
      <dc:creator>riteshpatel</dc:creator>
      <dc:date>2017-12-29T06:50:42Z</dc:date>
    </item>
  </channel>
</rss>