<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Yocto Linux L4.9.51 for i.MX 8MQuad GA release: imx-gpu-viv_6.2.4.p1.0 is broken for non-Wayland build configurations in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Linux-L4-9-51-for-i-MX-8MQuad-GA-release-imx-gpu-viv-6-2-4/m-p/752689#M117157</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It has been decided for the i.MX &lt;STRONG&gt;8M&lt;/STRONG&gt; to support wayland and xwayland. Neither fb nor X11 builds are supported. For the market the i.MX 8M&amp;nbsp; is targeted for, the X11 and fb setups had a lower priority, removing them reduced the implementation and testing effort for the BSP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may check the fsl-community for their strategy, currently the 8M is not in the list of supported platforms, but will for sure come.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bernhard.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 Jun 2018 10:51:57 GMT</pubDate>
    <dc:creator>bernhardfink</dc:creator>
    <dc:date>2018-06-18T10:51:57Z</dc:date>
    <item>
      <title>Yocto Linux L4.9.51 for i.MX 8MQuad GA release: imx-gpu-viv_6.2.4.p1.0 is broken for non-Wayland build configurations</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Linux-L4-9-51-for-i-MX-8MQuad-GA-release-imx-gpu-viv-6-2-4/m-p/752681#M117149</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm building the fsl-image-qt5-validation-imx image using 4.9.51 for i.MX 8MQuad GA release. My build is configured as below:&lt;/P&gt;&lt;P&gt;$ DISTRO=fsl-imx-fb MACHINE=imx8mqevk source fsl-setup-release.sh -b build-20180329&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The build fails in building the cairo package. The reason of the failure is that the pre-built shared library from the&amp;nbsp;imx-gpu-viv_6.2.4.p1.0 package contains reference to the Wayland library:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;psl@i7 build-20180329]$ readelf -d tmp/sysroots/imx8mqevk/usr/lib/gbm_viv.so&lt;/P&gt;&lt;P&gt;Dynamic section at offset 0x2888 contains 28 entries:&lt;BR /&gt; Tag Type Name/Value&lt;BR /&gt; 0x0000000000000001 (NEEDED) Shared library: [libdrm.so.2]&lt;BR /&gt; 0x0000000000000001 (NEEDED) Shared library: [libGAL.so]&lt;BR /&gt; 0x0000000000000001 (NEEDED) Shared library: [libwayland-server.so.0]&lt;BR /&gt; 0x0000000000000001 (NEEDED) Shared library: [libc.so.6]&lt;BR /&gt; 0x000000000000000e (SONAME) Library soname: [gbm_viv.so]&lt;BR /&gt; 0x000000000000000c (INIT) 0x1170&lt;BR /&gt;...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please advice.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Sergei&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 01 Apr 2018 07:34:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Linux-L4-9-51-for-i-MX-8MQuad-GA-release-imx-gpu-viv-6-2-4/m-p/752681#M117149</guid>
      <dc:creator>sergei_p</dc:creator>
      <dc:date>2018-04-01T07:34:32Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto Linux L4.9.51 for i.MX 8MQuad GA release: imx-gpu-viv_6.2.4.p1.0 is broken for non-Wayland build configurations</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Linux-L4-9-51-for-i-MX-8MQuad-GA-release-imx-gpu-viv-6-2-4/m-p/752682#M117150</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As I known, imx8m only supports wayland, so try to use the command as below, any error message, pls tell me&lt;/P&gt;&lt;P&gt;$ DISTRO=fsl-imx-xwayland MACHINE=imx8mqevk source fsl-setup-release.sh –b build-xwayland&lt;/P&gt;&lt;P&gt;$ DISTRO=fsl-imx-wayland MACHINE=imx8mqevk source fsl-setup-release.sh -b build-wayland&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Apr 2018 07:09:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Linux-L4-9-51-for-i-MX-8MQuad-GA-release-imx-gpu-viv-6-2-4/m-p/752682#M117150</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-04-04T07:09:18Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto Linux L4.9.51 for i.MX 8MQuad GA release: imx-gpu-viv_6.2.4.p1.0 is broken for non-Wayland build configurations</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Linux-L4-9-51-for-i-MX-8MQuad-GA-release-imx-gpu-viv-6-2-4/m-p/752683#M117151</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Joan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DISTRO=fsl-imx-x11 MACHINE=imx8mqevk source fsl-setup-release.sh -b build-20180329&lt;/P&gt;&lt;P&gt;Still the same build cairo package file&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/build-x11-20180402/tmp/sysroots/imx8mqevk/usr/lib/gbm_viv.so: undefined reference to `wl_resource_get_user_data'&lt;BR /&gt;| collect2: error: ld returned 1 exit status&lt;BR /&gt;| make[4]: *** [cairo-sphinx] Error 1&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Apr 2018 11:09:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Linux-L4-9-51-for-i-MX-8MQuad-GA-release-imx-gpu-viv-6-2-4/m-p/752683#M117151</guid>
      <dc:creator>Danube</dc:creator>
      <dc:date>2018-04-04T11:09:03Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto Linux L4.9.51 for i.MX 8MQuad GA release: imx-gpu-viv_6.2.4.p1.0 is broken for non-Wayland build configurations</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Linux-L4-9-51-for-i-MX-8MQuad-GA-release-imx-gpu-viv-6-2-4/m-p/752684#M117152</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I replied to you in your another case&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Apr 2018 03:18:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Linux-L4-9-51-for-i-MX-8MQuad-GA-release-imx-gpu-viv-6-2-4/m-p/752684#M117152</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-04-09T03:18:52Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto Linux L4.9.51 for i.MX 8MQuad GA release: imx-gpu-viv_6.2.4.p1.0 is broken for non-Wayland build configurations</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Linux-L4-9-51-for-i-MX-8MQuad-GA-release-imx-gpu-viv-6-2-4/m-p/752685#M117153</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please provide a link to the other case. I'm stuck on this issue also.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Apr 2018 00:06:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Linux-L4-9-51-for-i-MX-8MQuad-GA-release-imx-gpu-viv-6-2-4/m-p/752685#M117153</guid>
      <dc:creator>kendalla59</dc:creator>
      <dc:date>2018-04-19T00:06:37Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto Linux L4.9.51 for i.MX 8MQuad GA release: imx-gpu-viv_6.2.4.p1.0 is broken for non-Wayland build configurations</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Linux-L4-9-51-for-i-MX-8MQuad-GA-release-imx-gpu-viv-6-2-4/m-p/752686#M117154</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;as I mentioned, current bsp only supports wayland, not support X11 and fb&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Apr 2018 08:24:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Linux-L4-9-51-for-i-MX-8MQuad-GA-release-imx-gpu-viv-6-2-4/m-p/752686#M117154</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-04-19T08:24:34Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto Linux L4.9.51 for i.MX 8MQuad GA release: imx-gpu-viv_6.2.4.p1.0 is broken for non-Wayland build configurations</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Linux-L4-9-51-for-i-MX-8MQuad-GA-release-imx-gpu-viv-6-2-4/m-p/752687#M117155</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So to be explicitly clear, I must only use DISTRO=&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;fsl-imx-wayland&lt;/SPAN&gt;&amp;nbsp;for&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;MACHINE=imx8mqevk. Yes?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;May I assume that some time in the future, the bsp will support X11? Is there an estimate for the release of this support? &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;For me personally, I will never be critical of a support engineer being verbose or redundant when answering questions. Very short and cryptic answers however make searching for solutions more difficult.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Apr 2018 17:20:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Linux-L4-9-51-for-i-MX-8MQuad-GA-release-imx-gpu-viv-6-2-4/m-p/752687#M117155</guid>
      <dc:creator>kendalla59</dc:creator>
      <dc:date>2018-04-19T17:20:31Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto Linux L4.9.51 for i.MX 8MQuad GA release: imx-gpu-viv_6.2.4.p1.0 is broken for non-Wayland build configurations</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Linux-L4-9-51-for-i-MX-8MQuad-GA-release-imx-gpu-viv-6-2-4/m-p/752688#M117156</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kendall,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm also in the same situation.&lt;/P&gt;&lt;P&gt;I must evaluate our new IMX8 board, and though I'm noob with imx boards, I understand that the IMX8 community layers are not availables yet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So if I have understood your previous posts, the current official BSP does not support the fsl-imx-fb ?&lt;/P&gt;&lt;P&gt;Only wayland is supported ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually, I&amp;nbsp;just want to test our application built with Qt5.9 and run it with &lt;STRONG&gt;eglfs&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;But during the configuration of Qt5, eglfs backend is not selected as during the confiug tests, I experience the following error:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;imx8mqevk/usr/lib/gbm_viv.so: undefined reference to `wl_resource_get_user_data'&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Any update is welcome.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Thanks.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Karim&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 May 2018 15:25:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Linux-L4-9-51-for-i-MX-8MQuad-GA-release-imx-gpu-viv-6-2-4/m-p/752688#M117156</guid>
      <dc:creator>zyend</dc:creator>
      <dc:date>2018-05-31T15:25:12Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto Linux L4.9.51 for i.MX 8MQuad GA release: imx-gpu-viv_6.2.4.p1.0 is broken for non-Wayland build configurations</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Linux-L4-9-51-for-i-MX-8MQuad-GA-release-imx-gpu-viv-6-2-4/m-p/752689#M117157</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It has been decided for the i.MX &lt;STRONG&gt;8M&lt;/STRONG&gt; to support wayland and xwayland. Neither fb nor X11 builds are supported. For the market the i.MX 8M&amp;nbsp; is targeted for, the X11 and fb setups had a lower priority, removing them reduced the implementation and testing effort for the BSP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may check the fsl-community for their strategy, currently the 8M is not in the list of supported platforms, but will for sure come.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bernhard.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jun 2018 10:51:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Linux-L4-9-51-for-i-MX-8MQuad-GA-release-imx-gpu-viv-6-2-4/m-p/752689#M117157</guid>
      <dc:creator>bernhardfink</dc:creator>
      <dc:date>2018-06-18T10:51:57Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto Linux L4.9.51 for i.MX 8MQuad GA release: imx-gpu-viv_6.2.4.p1.0 is broken for non-Wayland build configurations</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Linux-L4-9-51-for-i-MX-8MQuad-GA-release-imx-gpu-viv-6-2-4/m-p/752690#M117158</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bernhard,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your feedback.&lt;/P&gt;&lt;P&gt;Would you please tell me which market exactly the iMX8M is targeted for ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Karim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jun 2018 11:57:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Linux-L4-9-51-for-i-MX-8MQuad-GA-release-imx-gpu-viv-6-2-4/m-p/752690#M117158</guid>
      <dc:creator>zyend</dc:creator>
      <dc:date>2018-06-21T11:57:36Z</dc:date>
    </item>
  </channel>
</rss>