<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: about i.mx6 solo H264 decoder</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/about-i-mx6-solo-H264-decoder/m-p/752656#M117145</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does anyone else have the same problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Jun 2018 03:13:29 GMT</pubDate>
    <dc:creator>liqun_wei</dc:creator>
    <dc:date>2018-06-13T03:13:29Z</dc:date>
    <item>
      <title>about i.mx6 solo H264 decoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/about-i-mx6-solo-H264-decoder/m-p/752655#M117144</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I got some h264 frames which can be decoded by CodecVisa and MPlayer and Elecard StreamEye,&lt;/P&gt;&lt;P&gt;when I send these frames to i.mx6, my system halted with white screen and here are some logs,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;sometimes the trace looks like this,&lt;/P&gt;&lt;P&gt;... ...&lt;/P&gt;&lt;P&gt;imx-ipuv3 2400000.ipu: IDMAC12's EBA0 is not 8-byte aligned&lt;BR /&gt;imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x40000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and sometimes the trace looks like this,&lt;/P&gt;&lt;P&gt;... ...&lt;/P&gt;&lt;P&gt;vpu_DecClrDispFlag failed Error code -3&lt;/P&gt;&lt;P&gt;imx-ipuv3 2400000.ipu: IDMAC12's EBA0 is not 8-byte aligned&lt;BR /&gt;imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x40000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've saved one stream.&lt;/P&gt;&lt;P&gt;Please refer the attachment file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestion will be very appreciated!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Jun 2018 10:25:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/about-i-mx6-solo-H264-decoder/m-p/752655#M117144</guid>
      <dc:creator>liqun_wei</dc:creator>
      <dc:date>2018-06-05T10:25:40Z</dc:date>
    </item>
    <item>
      <title>Re: about i.mx6 solo H264 decoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/about-i-mx6-solo-H264-decoder/m-p/752656#M117145</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does anyone else have the same problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jun 2018 03:13:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/about-i-mx6-solo-H264-decoder/m-p/752656#M117145</guid>
      <dc:creator>liqun_wei</dc:creator>
      <dc:date>2018-06-13T03:13:29Z</dc:date>
    </item>
    <item>
      <title>Re: about i.mx6 solo H264 decoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/about-i-mx6-solo-H264-decoder/m-p/752657#M117146</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi liqun,&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;According to the i.MX6(Q) Reference Manual :&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;IDMAC12's EBA0 is not 8-byte aligned, the file is not aligned.&lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt;"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;IPU_INT_STAT_10 = 0x00100000 means synchronous display error interrupt,&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;as a result of an error during access to a synchronous display.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&amp;nbsp;&amp;nbsp; Next, from section (Interrupt Generator) of the Reference Manual :&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;“The table below describes the error interrupts. The panic column indicates if this signal is&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;part of the logic generating the ipu_panic signal. The ipu_panic signal can be used for&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;indicating about errors that are result of data rate problems. Such problems may be a&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;result of the IPU running in slower clock then required by the use case. This signal can be&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;used in order to indicate the system that the IPU can't handle the desired data rate. In that&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;case the system may need to increase the clock to the IPU or simplify the use case.” &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&amp;nbsp;&amp;nbsp; So, we have here performance problem. Please try to decrease screen resolution and / or&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;frame rate. Also, other system resource consuming processes, such as USB / SD / SATA&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;transfer, may affect. As result a general performance issue may take place in the case. &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Perhaps it makes sense to try system prioritization (such as provided by Linux nice &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;command). &lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jun 2018 15:05:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/about-i-mx6-solo-H264-decoder/m-p/752657#M117146</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2018-06-25T15:05:23Z</dc:date>
    </item>
    <item>
      <title>Re: about i.mx6 solo H264 decoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/about-i-mx6-solo-H264-decoder/m-p/752658#M117147</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;&lt;P&gt;Additonal information, my display resolution is 1024x600.&lt;/P&gt;&lt;P&gt;In my case, I've met "&lt;SPAN style="font-size: 10.0pt;"&gt;not 8-byte aligned&lt;/SPAN&gt;" and "&lt;SPAN style="font-size: 10.0pt;"&gt;IPU_INT_STAT_10 = 0x00100000&lt;/SPAN&gt;" and also with nothing&lt;/P&gt;&lt;P&gt;display, the system freezes immediately.&lt;/P&gt;&lt;P&gt;And how to increase IPU clock?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jun 2018 03:30:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/about-i-mx6-solo-H264-decoder/m-p/752658#M117147</guid>
      <dc:creator>liqun_wei</dc:creator>
      <dc:date>2018-06-26T03:30:58Z</dc:date>
    </item>
    <item>
      <title>Re: about i.mx6 solo H264 decoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/about-i-mx6-solo-H264-decoder/m-p/752659#M117148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Finally, I found that we send two different resolution slice into VPU for the same decode session.&lt;/P&gt;&lt;P&gt;So that's the problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Apr 2019 07:12:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/about-i-mx6-solo-H264-decoder/m-p/752659#M117148</guid>
      <dc:creator>liqun_wei</dc:creator>
      <dc:date>2019-04-30T07:12:01Z</dc:date>
    </item>
  </channel>
</rss>