<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PC is not detecting NXP Imx6ul when connected in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PC-is-not-detecting-NXP-Imx6ul-when-connected/m-p/752365#M117078</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Please double check the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Check the proper functionality of USB cable.&lt;/LI&gt;&lt;LI&gt;Verify on which micro USB port is being connected the i.MX6UL base board: The one next to the standard Host port is the OTG port of the i.MX, while the one next to the power switch is the USB-to-serial converter.&lt;/LI&gt;&lt;LI&gt;Ensure that power supply is connected and providing 5V, and ensure turning on the base board with power switch.&lt;/LI&gt;&lt;LI&gt;Verify the boot configuration switches of the CPU board, in order to allow a correct booting, and also verify the proper locking of the SD card socket.&lt;/LI&gt;&lt;LI&gt;Ensure that booting SD card is properly working and that it was flashed with the correct image for i.MX6UL.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will be useful for you.&lt;/P&gt;&lt;P&gt;Best regards!&lt;/P&gt;&lt;P&gt;/Carlos&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Dec 2017 17:14:47 GMT</pubDate>
    <dc:creator>CarlosCasillas</dc:creator>
    <dc:date>2017-12-06T17:14:47Z</dc:date>
    <item>
      <title>PC is not detecting NXP Imx6ul when connected</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PC-is-not-detecting-NXP-Imx6ul-when-connected/m-p/752364#M117077</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I connected my Imx6ul to windows and Linux too but the Pc was unable to detect it&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Dec 2017 01:50:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PC-is-not-detecting-NXP-Imx6ul-when-connected/m-p/752364#M117077</guid>
      <dc:creator>omsriakashchint</dc:creator>
      <dc:date>2017-12-01T01:50:18Z</dc:date>
    </item>
    <item>
      <title>Re: PC is not detecting NXP Imx6ul when connected</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PC-is-not-detecting-NXP-Imx6ul-when-connected/m-p/752365#M117078</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Please double check the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Check the proper functionality of USB cable.&lt;/LI&gt;&lt;LI&gt;Verify on which micro USB port is being connected the i.MX6UL base board: The one next to the standard Host port is the OTG port of the i.MX, while the one next to the power switch is the USB-to-serial converter.&lt;/LI&gt;&lt;LI&gt;Ensure that power supply is connected and providing 5V, and ensure turning on the base board with power switch.&lt;/LI&gt;&lt;LI&gt;Verify the boot configuration switches of the CPU board, in order to allow a correct booting, and also verify the proper locking of the SD card socket.&lt;/LI&gt;&lt;LI&gt;Ensure that booting SD card is properly working and that it was flashed with the correct image for i.MX6UL.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will be useful for you.&lt;/P&gt;&lt;P&gt;Best regards!&lt;/P&gt;&lt;P&gt;/Carlos&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Dec 2017 17:14:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PC-is-not-detecting-NXP-Imx6ul-when-connected/m-p/752365#M117078</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2017-12-06T17:14:47Z</dc:date>
    </item>
  </channel>
</rss>