<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: adding kernel paches to imx7d picopi yocto</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/adding-kernel-paches-to-imx7d-picopi-yocto/m-p/751984#M117038</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, I got it working. I had to change recipe to use newer head of the kernel. Dunno why the workarea linux as one the layers didn't work. Perhaps some other layer used different kernel version or something.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 19 Feb 2018 13:04:55 GMT</pubDate>
    <dc:creator>maash</dc:creator>
    <dc:date>2018-02-19T13:04:55Z</dc:date>
    <item>
      <title>adding kernel paches to imx7d picopi yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/adding-kernel-paches-to-imx7d-picopi-yocto/m-p/751983#M117037</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the picopi with yocto and trying to add some kernel patches to my package. I've watched several tutorials, read the yocto project tutorials, but I'm still a bit baffled what goes wrong.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I've got meta-avs-demos -project from NXP codeaurora. It compiles OK out of box.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However I cannot seem to be able to patch the kernel and then do the full build.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've followed these instructions to get the kernel sources, add the pathes and make successful build:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://wiki.yoctoproject.org/wiki/TipsAndTricks/Patching_the_source_for_a_recipe" title="https://wiki.yoctoproject.org/wiki/TipsAndTricks/Patching_the_source_for_a_recipe"&gt;TipsAndTricks/Patching the source for a recipe - Yocto Project&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And that amounts to basically:&lt;/P&gt;&lt;P&gt;devtool modify linux-imx&lt;/P&gt;&lt;P&gt;cd workspace/sources/linux-imx/&lt;/P&gt;&lt;P&gt;checkout tn-imx_4.1.15_2.0.0_ga&lt;/P&gt;&lt;P&gt;git pull&lt;/P&gt;&lt;P&gt;git am /path/to/paches&lt;/P&gt;&lt;P&gt;bitbake linux-imx&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This builds OK.&lt;/P&gt;&lt;P&gt;However if I try then make the whole package bitbake avs-image, this fails:&lt;/P&gt;&lt;P&gt;BB_VERSION = "1.30.0"&lt;BR /&gt;BUILD_SYS = "x86_64-linux"&lt;BR /&gt;NATIVELSBSTRING = "Ubuntu-14.04"&lt;BR /&gt;TARGET_SYS = "arm-poky-linux-gnueabi"&lt;BR /&gt;MACHINE = "imx7d-pico"&lt;BR /&gt;DISTRO = "fsl-imx-x11"&lt;BR /&gt;DISTRO_VERSION = "4.1.15-2.1.0"&lt;BR /&gt;TUNE_FEATURES = "arm armv7ve vfp neon callconvention-hard cortexa7"&lt;BR /&gt;TARGET_FPU = "hard"&lt;/P&gt;&lt;P&gt;....&lt;/P&gt;&lt;P&gt;ERROR: Task do_unpack in /home/build/workspace/sources/poky/meta/recipes-kernel/perf/perf.bb depends upon non-existent task do_patch in /home/build/workspace/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux/linux-imx_4.1.15.bb&lt;BR /&gt;ERROR: Command execution failed: 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried adding the stuff to layer (which is why I would like get this working in the first place), however it also fails.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Feb 2018 14:25:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/adding-kernel-paches-to-imx7d-picopi-yocto/m-p/751983#M117037</guid>
      <dc:creator>maash</dc:creator>
      <dc:date>2018-02-16T14:25:28Z</dc:date>
    </item>
    <item>
      <title>Re: adding kernel paches to imx7d picopi yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/adding-kernel-paches-to-imx7d-picopi-yocto/m-p/751984#M117038</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, I got it working. I had to change recipe to use newer head of the kernel. Dunno why the workarea linux as one the layers didn't work. Perhaps some other layer used different kernel version or something.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Feb 2018 13:04:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/adding-kernel-paches-to-imx7d-picopi-yocto/m-p/751984#M117038</guid>
      <dc:creator>maash</dc:creator>
      <dc:date>2018-02-19T13:04:55Z</dc:date>
    </item>
  </channel>
</rss>