<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: imx rt1050 camera issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx-rt1050-camera-issue/m-p/750101#M116731</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;UL&gt;&lt;LI&gt;&lt;H6&gt;pls use the SDK to test first, the user case in the sdk named graphic, which use case will use CSI, PXP and LCD to achieve a viewfinder which can be save the image from the camera into JPEG file and save to SD card.&lt;/H6&gt;&lt;H6&gt;&lt;SPAN style="font-size: 20pt; color: black;"&gt;&lt;BR style="font-size: 20pt; color: black;" /&gt;&lt;/SPAN&gt;&lt;/H6&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 Feb 2018 09:07:51 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2018-02-02T09:07:51Z</dc:date>
    <item>
      <title>imx rt1050 camera issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-rt1050-camera-issue/m-p/750100#M116730</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on imx rt1050 evk.I tried flashing default camera example from the below path:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;C:\i.MXRT1050-Example-Code-and-HW-Guide\i.MXRT1050 EVK Extension Feature Example Code and HW Guide\CSI\boards\evkmimxrt1050\driver_examples\csi\rgb565&amp;nbsp; &amp;nbsp;using IAR.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Only backlight for LCD comes up.nothing comes up on LCD.&lt;/P&gt;&lt;P&gt;Camera images are not displayed on LCD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What will be the issue ?&lt;/P&gt;&lt;P&gt;How can we check LCD and camera are working fine?&lt;/P&gt;&lt;P&gt;Is there any LCD example to check if it is working fine for imx rt1050?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;P&gt;Rizwan Syed&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jan 2018 13:24:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-rt1050-camera-issue/m-p/750100#M116730</guid>
      <dc:creator>rizwan_s</dc:creator>
      <dc:date>2018-01-23T13:24:01Z</dc:date>
    </item>
    <item>
      <title>Re: imx rt1050 camera issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-rt1050-camera-issue/m-p/750101#M116731</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;UL&gt;&lt;LI&gt;&lt;H6&gt;pls use the SDK to test first, the user case in the sdk named graphic, which use case will use CSI, PXP and LCD to achieve a viewfinder which can be save the image from the camera into JPEG file and save to SD card.&lt;/H6&gt;&lt;H6&gt;&lt;SPAN style="font-size: 20pt; color: black;"&gt;&lt;BR style="font-size: 20pt; color: black;" /&gt;&lt;/SPAN&gt;&lt;/H6&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Feb 2018 09:07:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-rt1050-camera-issue/m-p/750101#M116731</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-02-02T09:07:51Z</dc:date>
    </item>
    <item>
      <title>Re: imx rt1050 camera issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-rt1050-camera-issue/m-p/750102#M116732</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Joan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did you mean the example was included in MCUXpresso SDK?&lt;/P&gt;&lt;P&gt;Was it also&amp;nbsp;have MCUXpresso IDE support?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Feb 2018 02:47:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-rt1050-camera-issue/m-p/750102#M116732</guid>
      <dc:creator>kyleyang</dc:creator>
      <dc:date>2018-02-05T02:47:00Z</dc:date>
    </item>
    <item>
      <title>Re: imx rt1050 camera issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-rt1050-camera-issue/m-p/750103#M116733</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;When using the camera on Rev. A of i.MX RT EVK boards, it will be required to add 0-ohm resistors on R217, R218, R220, R221, R222, R223, R224, R225, R226, R227, R228 and R229, as mentioned on “MIMXRT1050 EVK Board Hardware User’s Guide” document.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will be useful for you.Best regards!&lt;/P&gt;&lt;P&gt;/Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Feb 2018 23:34:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-rt1050-camera-issue/m-p/750103#M116733</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2018-02-21T23:34:06Z</dc:date>
    </item>
    <item>
      <title>Re: imx rt1050 camera issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-rt1050-camera-issue/m-p/750104#M116734</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi may i know what camera module you are using@&lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="230114" data-username="rizwansyed" href="https://community.nxp.com/people/rizwansyed"&gt;rizwan syed&lt;/A&gt;? with the specific part number and if possible the link to purchase the camera module too.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 May 2018 08:41:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-rt1050-camera-issue/m-p/750104#M116734</guid>
      <dc:creator>mingyang</dc:creator>
      <dc:date>2018-05-08T08:41:53Z</dc:date>
    </item>
    <item>
      <title>Re: imx rt1050 camera issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-rt1050-camera-issue/m-p/750105#M116735</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;may i know the timeline for the release of the camera code for mt9m114 similar to the ov7725 &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 May 2018 09:23:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-rt1050-camera-issue/m-p/750105#M116735</guid>
      <dc:creator>mingyang</dc:creator>
      <dc:date>2018-05-08T09:23:01Z</dc:date>
    </item>
  </channel>
</rss>