<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 SDHC Class 10 Boot -Processor Part Number?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SDHC-Class-10-Boot-Processor-Part-Number/m-p/750069#M116726</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can somebody Suggest a Processor which can have a SDHC card has a boot interface?&lt;/P&gt;&lt;P&gt;UART-3&lt;/P&gt;&lt;P&gt;SPI-2&lt;/P&gt;&lt;P&gt;ADC-2.&lt;/P&gt;&lt;P&gt;JTAG&lt;/P&gt;&lt;P&gt;ADC-2&lt;/P&gt;&lt;P&gt;Secondary Boot&lt;/P&gt;&lt;P&gt;SRAM min-512KB&lt;/P&gt;&lt;P&gt;SDHC-Transfer speed 10MB/s should support class 10&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;----------------&lt;/P&gt;&lt;P&gt;DDR2- if available not manadatory&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see no micro controller doing SDHC boot from my trade study.&lt;/P&gt;&lt;P&gt;But a micro controller is can do all except SDHC boot with boot options to the next boot device no bootstrap is available on it?.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help or suggestions of part numbers?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Mar 2018 15:09:35 GMT</pubDate>
    <dc:creator>balajipadmanaba</dc:creator>
    <dc:date>2018-03-12T15:09:35Z</dc:date>
    <item>
      <title>SDHC Class 10 Boot -Processor Part Number?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SDHC-Class-10-Boot-Processor-Part-Number/m-p/750069#M116726</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can somebody Suggest a Processor which can have a SDHC card has a boot interface?&lt;/P&gt;&lt;P&gt;UART-3&lt;/P&gt;&lt;P&gt;SPI-2&lt;/P&gt;&lt;P&gt;ADC-2.&lt;/P&gt;&lt;P&gt;JTAG&lt;/P&gt;&lt;P&gt;ADC-2&lt;/P&gt;&lt;P&gt;Secondary Boot&lt;/P&gt;&lt;P&gt;SRAM min-512KB&lt;/P&gt;&lt;P&gt;SDHC-Transfer speed 10MB/s should support class 10&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;----------------&lt;/P&gt;&lt;P&gt;DDR2- if available not manadatory&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see no micro controller doing SDHC boot from my trade study.&lt;/P&gt;&lt;P&gt;But a micro controller is can do all except SDHC boot with boot options to the next boot device no bootstrap is available on it?.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help or suggestions of part numbers?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Mar 2018 15:09:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SDHC-Class-10-Boot-Processor-Part-Number/m-p/750069#M116726</guid>
      <dc:creator>balajipadmanaba</dc:creator>
      <dc:date>2018-03-12T15:09:35Z</dc:date>
    </item>
    <item>
      <title>Re: SDHC Class 10 Boot -Processor Part Number?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SDHC-Class-10-Boot-Processor-Part-Number/m-p/750070#M116727</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi balaji&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check i.MX comparison table&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/brochure/FLYRIMXPRDCMPR.pdf" title="https://www.nxp.com/docs/en/brochure/FLYRIMXPRDCMPR.pdf"&gt;https://www.nxp.com/docs/en/brochure/FLYRIMXPRDCMPR.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Mar 2018 22:58:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SDHC-Class-10-Boot-Processor-Part-Number/m-p/750070#M116727</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-03-12T22:58:47Z</dc:date>
    </item>
  </channel>
</rss>