<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX 8M DMA Support for Cortex-M4 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-DMA-Support-for-Cortex-M4/m-p/749563#M116655</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Greetings,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the i.MX6 and i.MX7 processors&amp;nbsp;the SDMA controller is a shared peripheral between the Cortex-A and Cortex-M processors; but Linux is essentially crippled without DMA; so the Cortex-M effectively can never use DMA while using Linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the i.MX 8M block diagram it shows 2x SDMA controllers.&amp;nbsp;Will it be possible to have one of these available for the Cortex-M processor; or will Linux demand both of them?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;- Malcolm&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Dec 2017 16:37:03 GMT</pubDate>
    <dc:creator>malcolmnixon</dc:creator>
    <dc:date>2017-12-27T16:37:03Z</dc:date>
    <item>
      <title>i.MX 8M DMA Support for Cortex-M4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-DMA-Support-for-Cortex-M4/m-p/749563#M116655</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Greetings,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the i.MX6 and i.MX7 processors&amp;nbsp;the SDMA controller is a shared peripheral between the Cortex-A and Cortex-M processors; but Linux is essentially crippled without DMA; so the Cortex-M effectively can never use DMA while using Linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the i.MX 8M block diagram it shows 2x SDMA controllers.&amp;nbsp;Will it be possible to have one of these available for the Cortex-M processor; or will Linux demand both of them?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;- Malcolm&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Dec 2017 16:37:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-DMA-Support-for-Cortex-M4/m-p/749563#M116655</guid>
      <dc:creator>malcolmnixon</dc:creator>
      <dc:date>2017-12-27T16:37:03Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M DMA Support for Cortex-M4</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-DMA-Support-for-Cortex-M4/m-p/749564#M116656</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Unfortunately we are not able to talk details about the i.MX8M since it is not release yet, and can be subject to changes, but at the moment, I can said that both SDMA are not intended for the M4.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Merry Christmas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Dec 2017 20:05:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-DMA-Support-for-Cortex-M4/m-p/749564#M116656</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2017-12-28T20:05:20Z</dc:date>
    </item>
  </channel>
</rss>