<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX28 FEC Testing</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-FEC-Testing/m-p/749104#M116546</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have been doing some network testing on an i.MX28 running 2.6.35_maintain kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems that even on a point-to-point connection, there are many TCP re-transmissions from the host PC, and occasionally duplicate ACKs from the i.MX. Using Wireshark to monitor traffic, it will also give warnings that the receiver (i.MX) TCP window is full.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This seems to indicate that the i.MX is not handling packets fast enough. Is this an issue that has been seen and addressed before? Any help is appreciated.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Some other details:&lt;/P&gt;&lt;P&gt;Testing done with iperf3&lt;/P&gt;&lt;P&gt;i.MX on eth0 – hardware based on EVK design&lt;/P&gt;&lt;P&gt;2.6.35_maintain kernel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Mar 2018 13:44:49 GMT</pubDate>
    <dc:creator>jkuz</dc:creator>
    <dc:date>2018-03-12T13:44:49Z</dc:date>
    <item>
      <title>i.MX28 FEC Testing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-FEC-Testing/m-p/749104#M116546</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have been doing some network testing on an i.MX28 running 2.6.35_maintain kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems that even on a point-to-point connection, there are many TCP re-transmissions from the host PC, and occasionally duplicate ACKs from the i.MX. Using Wireshark to monitor traffic, it will also give warnings that the receiver (i.MX) TCP window is full.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This seems to indicate that the i.MX is not handling packets fast enough. Is this an issue that has been seen and addressed before? Any help is appreciated.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Some other details:&lt;/P&gt;&lt;P&gt;Testing done with iperf3&lt;/P&gt;&lt;P&gt;i.MX on eth0 – hardware based on EVK design&lt;/P&gt;&lt;P&gt;2.6.35_maintain kernel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Mar 2018 13:44:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-FEC-Testing/m-p/749104#M116546</guid>
      <dc:creator>jkuz</dc:creator>
      <dc:date>2018-03-12T13:44:49Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX28 FEC Testing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-FEC-Testing/m-p/749105#M116547</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please check if the hardware (cable, etc) is OK.&lt;BR /&gt;Also please note that i.MX series are more multimedia than networking processors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Mar 2018 09:22:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-FEC-Testing/m-p/749105#M116547</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2018-03-15T09:22:45Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX28 FEC Testing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX28-FEC-Testing/m-p/749106#M116548</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jason,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kernel 2.6.35 is no longer supported. I suggest you to try a recent kernel on mx28, such as 4.15.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Mar 2018 13:13:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX28-FEC-Testing/m-p/749106#M116548</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2018-03-15T13:13:25Z</dc:date>
    </item>
  </channel>
</rss>