<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックMaking cpu reset cause available from U-Boot to Linux</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Making-cpu-reset-cause-available-from-U-Boot-to-Linux/m-p/748637#M116460</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'd like the system's reset cause (por, watchdog etc) to be available to Linux - it's shown in the u-boot debug e.g.&lt;/P&gt;&lt;P&gt;"Reset cause: POR"&lt;/P&gt;&lt;P&gt;I've only found a few references to this in searching, and it seems that u-boot clears the register after reading?&lt;/P&gt;&lt;P&gt;Has anyone done any modifications to preserve this, and then been able to read it from the OS?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Dec 2017 16:15:05 GMT</pubDate>
    <dc:creator>colinhelliwell</dc:creator>
    <dc:date>2017-12-27T16:15:05Z</dc:date>
    <item>
      <title>Making cpu reset cause available from U-Boot to Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Making-cpu-reset-cause-available-from-U-Boot-to-Linux/m-p/748637#M116460</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'd like the system's reset cause (por, watchdog etc) to be available to Linux - it's shown in the u-boot debug e.g.&lt;/P&gt;&lt;P&gt;"Reset cause: POR"&lt;/P&gt;&lt;P&gt;I've only found a few references to this in searching, and it seems that u-boot clears the register after reading?&lt;/P&gt;&lt;P&gt;Has anyone done any modifications to preserve this, and then been able to read it from the OS?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Dec 2017 16:15:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Making-cpu-reset-cause-available-from-U-Boot-to-Linux/m-p/748637#M116460</guid>
      <dc:creator>colinhelliwell</dc:creator>
      <dc:date>2017-12-27T16:15:05Z</dc:date>
    </item>
    <item>
      <title>Re: Making cpu reset cause available from U-Boot to Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Making-cpu-reset-cause-available-from-U-Boot-to-Linux/m-p/748638#M116461</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi colinhelliwell&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems you are right, in general one can save that reset info in some&lt;BR /&gt;of SRC_GPR registers and use in linux.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Dec 2017 05:21:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Making-cpu-reset-cause-available-from-U-Boot-to-Linux/m-p/748638#M116461</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-12-28T05:21:49Z</dc:date>
    </item>
  </channel>
</rss>