<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックWandboard PCIE support</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Wandboard-PCIE-support/m-p/748625#M116455</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all&lt;BR /&gt;i have a wandboard with EDM1-IMX6-sd REV A1 som board. i just need to enable the PCIE support in kernel config and dtb . this is for interfacing a WiFi card with PCIE support. From WiFi card PCIE TX, RX, CLK and PCI_RST lines are connected. PCI_CLK_RQT and PCI_WAKE aren't connected.&amp;nbsp;&lt;BR /&gt;For dtb i tried following change&lt;BR /&gt;+&amp;amp;pcie {&lt;BR /&gt;+ pinctrl-names = "default";&lt;BR /&gt;+ pinctrl-0 = &amp;lt;&amp;amp;pinctrl_pcie&amp;gt;;&lt;BR /&gt;+ reset-gpio = &amp;lt;&amp;amp;gpio3 31 1&amp;gt;;&lt;BR /&gt;+ status = "okay";&lt;BR /&gt;+};&lt;BR /&gt;for kernel defconfig followed the Linux reference manual 4.1.15 &lt;BR /&gt;#&lt;BR /&gt;# Bus support&lt;BR /&gt;#&lt;BR /&gt;CONFIG_PCI=y&lt;BR /&gt;CONFIG_PCI_DOMAINS=y&lt;BR /&gt;CONFIG_PCI_SYSCALL=y&lt;BR /&gt;CONFIG_PCI_MSI=y&lt;BR /&gt;#&lt;BR /&gt;# PCI host controller drivers&lt;BR /&gt;#&lt;BR /&gt;CONFIG_PCIE_DW=y&lt;BR /&gt;CONFIG_PCI_IMX6=y&lt;/P&gt;&lt;P&gt;But when boots up kernel print shows &lt;BR /&gt;imx6q-pcie 1ffc000.pcie: phy link never came up&lt;BR /&gt;imx6q-pcie 1ffc000.pcie: DEBUG_R0: 0x00023600, DEBUG_R1: 0x08200000&lt;BR /&gt;imx6q-pcie 1ffc000.pcie: failed to initialize host&lt;BR /&gt;imx6q-pcie: probe of 1ffc000.pcie failed with error -22&lt;/P&gt;&lt;P&gt;i also tried the kernel configuration suggested in &lt;A _jive_internal="true" href="https://community.nxp.com/forums.wandboard.org/viewtopic.php?f=8&amp;amp;t=902, still same prints Is i am missing anything in kernel configuration ? Please suggest, any help is welcomed"&gt;http://forums.wandboard.org/viewtopic.php?f=8&amp;amp;t=902,&lt;/A&gt; still same prints.&lt;BR /&gt;Is i am missing anything in kernel configuration ? Please suggest, any help is welcomed&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Jan 2018 13:04:24 GMT</pubDate>
    <dc:creator>anjojohn</dc:creator>
    <dc:date>2018-01-23T13:04:24Z</dc:date>
    <item>
      <title>Wandboard PCIE support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Wandboard-PCIE-support/m-p/748625#M116455</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all&lt;BR /&gt;i have a wandboard with EDM1-IMX6-sd REV A1 som board. i just need to enable the PCIE support in kernel config and dtb . this is for interfacing a WiFi card with PCIE support. From WiFi card PCIE TX, RX, CLK and PCI_RST lines are connected. PCI_CLK_RQT and PCI_WAKE aren't connected.&amp;nbsp;&lt;BR /&gt;For dtb i tried following change&lt;BR /&gt;+&amp;amp;pcie {&lt;BR /&gt;+ pinctrl-names = "default";&lt;BR /&gt;+ pinctrl-0 = &amp;lt;&amp;amp;pinctrl_pcie&amp;gt;;&lt;BR /&gt;+ reset-gpio = &amp;lt;&amp;amp;gpio3 31 1&amp;gt;;&lt;BR /&gt;+ status = "okay";&lt;BR /&gt;+};&lt;BR /&gt;for kernel defconfig followed the Linux reference manual 4.1.15 &lt;BR /&gt;#&lt;BR /&gt;# Bus support&lt;BR /&gt;#&lt;BR /&gt;CONFIG_PCI=y&lt;BR /&gt;CONFIG_PCI_DOMAINS=y&lt;BR /&gt;CONFIG_PCI_SYSCALL=y&lt;BR /&gt;CONFIG_PCI_MSI=y&lt;BR /&gt;#&lt;BR /&gt;# PCI host controller drivers&lt;BR /&gt;#&lt;BR /&gt;CONFIG_PCIE_DW=y&lt;BR /&gt;CONFIG_PCI_IMX6=y&lt;/P&gt;&lt;P&gt;But when boots up kernel print shows &lt;BR /&gt;imx6q-pcie 1ffc000.pcie: phy link never came up&lt;BR /&gt;imx6q-pcie 1ffc000.pcie: DEBUG_R0: 0x00023600, DEBUG_R1: 0x08200000&lt;BR /&gt;imx6q-pcie 1ffc000.pcie: failed to initialize host&lt;BR /&gt;imx6q-pcie: probe of 1ffc000.pcie failed with error -22&lt;/P&gt;&lt;P&gt;i also tried the kernel configuration suggested in &lt;A _jive_internal="true" href="https://community.nxp.com/forums.wandboard.org/viewtopic.php?f=8&amp;amp;t=902, still same prints Is i am missing anything in kernel configuration ? Please suggest, any help is welcomed"&gt;http://forums.wandboard.org/viewtopic.php?f=8&amp;amp;t=902,&lt;/A&gt; still same prints.&lt;BR /&gt;Is i am missing anything in kernel configuration ? Please suggest, any help is welcomed&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jan 2018 13:04:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Wandboard-PCIE-support/m-p/748625#M116455</guid>
      <dc:creator>anjojohn</dc:creator>
      <dc:date>2018-01-23T13:04:24Z</dc:date>
    </item>
    <item>
      <title>Re: Wandboard PCIE support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Wandboard-PCIE-support/m-p/748626#M116456</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Anjo John,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would recommend you posting your question on Wandboard forums as well, as there may be more users with valuable input there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/wandboard"&gt;wandboard&lt;/A&gt;, would you please let us know if there’s any suggestion for PCIE support on this board?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jan 2018 20:37:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Wandboard-PCIE-support/m-p/748626#M116456</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2018-01-23T20:37:06Z</dc:date>
    </item>
  </channel>
</rss>