<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic eMMC Flash partition READ-WRITE from Read Only in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-Flash-partition-READ-WRITE-from-Read-Only/m-p/748576#M116443</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please find below details and query.&lt;/P&gt;&lt;P&gt;~ # fdisk -l&lt;/P&gt;&lt;P&gt;Disk /dev/mmcblk0: 116 MB, 116523008 bytes&lt;BR /&gt;4 heads, 16 sectors/track, 3556 cylinders&lt;BR /&gt;Units = cylinders of 64 * 512 = 32768 bytes&lt;/P&gt;&lt;P&gt;Device Boot Start End Blocks Id System&lt;BR /&gt;/dev/mmcblk0p1 73 200 4096 83 Linux&lt;BR /&gt;/dev/mmcblk0p2 201 328 4096 83 Linux&lt;BR /&gt;/dev/mmcblk0p3 329 872 17408 83 Linux&lt;BR /&gt;/dev/mmcblk0p4 873 3556 85888 5 Extended&lt;BR /&gt;/dev/mmcblk0p5 877 1420 17408 83 Linux&lt;BR /&gt;/dev/mmcblk0p6 1425 1488 2048 83 Linux&lt;BR /&gt;/dev/mmcblk0p7 1493 1556 2048 83 Linux&lt;BR /&gt;/dev/mmcblk0p8 1573 1668 3072 83 Linux&lt;BR /&gt;/dev/mmcblk0p9 1673 1768 3072 83 Linux&lt;BR /&gt;/dev/mmcblk0p10 1773 1836 2048 83 Linux&lt;BR /&gt;/dev/mmcblk0p11 1841 1904 2048 83 Linux&lt;BR /&gt;/dev/mmcblk0p12 1909 2196 9216 83 Linux&lt;BR /&gt;/dev/mmcblk0p13 2201 2488 9216 83 Linux&lt;BR /&gt;/dev/mmcblk0p14 2493 2940 14336 83 Linux&lt;BR /&gt;/dev/mmcblk0p15 2945 3392 14336 83 Linux&lt;/P&gt;&lt;P&gt;The Partition /dev/mmcblk0p13 which is used for rootfs. But it is in Read-Only mode.&lt;/P&gt;&lt;P&gt;For debugging purpose, I need to change Read-Write permission for /dev/mmcblk0p13.&lt;/P&gt;&lt;P&gt;Can you please share the procedure to convert to Read-Write?&lt;/P&gt;&lt;P&gt;The Partition /dev/mmcblk0p13 which is based on squashfs.&lt;/P&gt;&lt;P&gt;~ # mount&lt;BR /&gt;/dev/root on / type squashfs (ro,relatime)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Please share your inputs.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Nov 2017 11:55:35 GMT</pubDate>
    <dc:creator>mselvara82</dc:creator>
    <dc:date>2017-11-03T11:55:35Z</dc:date>
    <item>
      <title>eMMC Flash partition READ-WRITE from Read Only</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-Flash-partition-READ-WRITE-from-Read-Only/m-p/748576#M116443</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please find below details and query.&lt;/P&gt;&lt;P&gt;~ # fdisk -l&lt;/P&gt;&lt;P&gt;Disk /dev/mmcblk0: 116 MB, 116523008 bytes&lt;BR /&gt;4 heads, 16 sectors/track, 3556 cylinders&lt;BR /&gt;Units = cylinders of 64 * 512 = 32768 bytes&lt;/P&gt;&lt;P&gt;Device Boot Start End Blocks Id System&lt;BR /&gt;/dev/mmcblk0p1 73 200 4096 83 Linux&lt;BR /&gt;/dev/mmcblk0p2 201 328 4096 83 Linux&lt;BR /&gt;/dev/mmcblk0p3 329 872 17408 83 Linux&lt;BR /&gt;/dev/mmcblk0p4 873 3556 85888 5 Extended&lt;BR /&gt;/dev/mmcblk0p5 877 1420 17408 83 Linux&lt;BR /&gt;/dev/mmcblk0p6 1425 1488 2048 83 Linux&lt;BR /&gt;/dev/mmcblk0p7 1493 1556 2048 83 Linux&lt;BR /&gt;/dev/mmcblk0p8 1573 1668 3072 83 Linux&lt;BR /&gt;/dev/mmcblk0p9 1673 1768 3072 83 Linux&lt;BR /&gt;/dev/mmcblk0p10 1773 1836 2048 83 Linux&lt;BR /&gt;/dev/mmcblk0p11 1841 1904 2048 83 Linux&lt;BR /&gt;/dev/mmcblk0p12 1909 2196 9216 83 Linux&lt;BR /&gt;/dev/mmcblk0p13 2201 2488 9216 83 Linux&lt;BR /&gt;/dev/mmcblk0p14 2493 2940 14336 83 Linux&lt;BR /&gt;/dev/mmcblk0p15 2945 3392 14336 83 Linux&lt;/P&gt;&lt;P&gt;The Partition /dev/mmcblk0p13 which is used for rootfs. But it is in Read-Only mode.&lt;/P&gt;&lt;P&gt;For debugging purpose, I need to change Read-Write permission for /dev/mmcblk0p13.&lt;/P&gt;&lt;P&gt;Can you please share the procedure to convert to Read-Write?&lt;/P&gt;&lt;P&gt;The Partition /dev/mmcblk0p13 which is based on squashfs.&lt;/P&gt;&lt;P&gt;~ # mount&lt;BR /&gt;/dev/root on / type squashfs (ro,relatime)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Please share your inputs.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Nov 2017 11:55:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/eMMC-Flash-partition-READ-WRITE-from-Read-Only/m-p/748576#M116443</guid>
      <dc:creator>mselvara82</dc:creator>
      <dc:date>2017-11-03T11:55:35Z</dc:date>
    </item>
  </channel>
</rss>