<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic OpenCL1.2 Full Profile on QuadPlus in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/OpenCL1-2-Full-Profile-on-QuadPlus/m-p/748291#M116367</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;The QP is supposed to support OpenCL full profile from driver 6.2.2p0, but I can’t seem to make it work any pointers?, I’m getting this from clinfo:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ptr: 0x0093f698&lt;BR /&gt; CL_DEVICE_NAME: Vivante OpenCL Device GC3000.5450.0000&lt;BR /&gt; CL_DEVICE_VENDOR: Vivante Corporation&lt;BR /&gt; CL_DEVICE_TYPE: GPU &lt;BR /&gt; CL_DEVICE_OPENCL_C_VERSION: OpenCL C 1.1 &lt;BR /&gt; CL_DEVICE_VENDOR_ID: 0x00564956&lt;BR /&gt; CL_DEVICE_PLATFORM: 0xa602eaf4&lt;BR /&gt; CL_DEVICE_VERSION: OpenCL 1.1 &lt;BR /&gt; CL_DEVICE_PROFILE: EMBEDDED_PROFILE&lt;BR /&gt; CL_DRIVER_VERSION: OpenCL 1.1 V6.2.2.93313&lt;BR /&gt; CL_DEVICE_MAX_COMPUTE_UNITS: 4&lt;BR /&gt; CL_DEVICE_MAX_WORK_ITEM_DIMENSIONS: 3&lt;BR /&gt; CL_DEVICE_MAX_WORK_ITEM_SIZES[0]: 1024&lt;BR /&gt; CL_DEVICE_MAX_WORK_ITEM_SIZES[1]: 1024&lt;BR /&gt; CL_DEVICE_MAX_WORK_ITEM_SIZES[2]: 1024&lt;BR /&gt; CL_DEVICE_MAX_WORK_GROUP_SIZE: 1024&lt;BR /&gt; CL_DEVICE_MAX_CLOCK_FREQUENCY: 500 MHz&lt;BR /&gt; CL_DEVICE_IMAGE_SUPPORT: Yes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 13 May 2018 23:24:22 GMT</pubDate>
    <dc:creator>tequilaguur</dc:creator>
    <dc:date>2018-05-13T23:24:22Z</dc:date>
    <item>
      <title>OpenCL1.2 Full Profile on QuadPlus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/OpenCL1-2-Full-Profile-on-QuadPlus/m-p/748291#M116367</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;The QP is supposed to support OpenCL full profile from driver 6.2.2p0, but I can’t seem to make it work any pointers?, I’m getting this from clinfo:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ptr: 0x0093f698&lt;BR /&gt; CL_DEVICE_NAME: Vivante OpenCL Device GC3000.5450.0000&lt;BR /&gt; CL_DEVICE_VENDOR: Vivante Corporation&lt;BR /&gt; CL_DEVICE_TYPE: GPU &lt;BR /&gt; CL_DEVICE_OPENCL_C_VERSION: OpenCL C 1.1 &lt;BR /&gt; CL_DEVICE_VENDOR_ID: 0x00564956&lt;BR /&gt; CL_DEVICE_PLATFORM: 0xa602eaf4&lt;BR /&gt; CL_DEVICE_VERSION: OpenCL 1.1 &lt;BR /&gt; CL_DEVICE_PROFILE: EMBEDDED_PROFILE&lt;BR /&gt; CL_DRIVER_VERSION: OpenCL 1.1 V6.2.2.93313&lt;BR /&gt; CL_DEVICE_MAX_COMPUTE_UNITS: 4&lt;BR /&gt; CL_DEVICE_MAX_WORK_ITEM_DIMENSIONS: 3&lt;BR /&gt; CL_DEVICE_MAX_WORK_ITEM_SIZES[0]: 1024&lt;BR /&gt; CL_DEVICE_MAX_WORK_ITEM_SIZES[1]: 1024&lt;BR /&gt; CL_DEVICE_MAX_WORK_ITEM_SIZES[2]: 1024&lt;BR /&gt; CL_DEVICE_MAX_WORK_GROUP_SIZE: 1024&lt;BR /&gt; CL_DEVICE_MAX_CLOCK_FREQUENCY: 500 MHz&lt;BR /&gt; CL_DEVICE_IMAGE_SUPPORT: Yes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 13 May 2018 23:24:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/OpenCL1-2-Full-Profile-on-QuadPlus/m-p/748291#M116367</guid>
      <dc:creator>tequilaguur</dc:creator>
      <dc:date>2018-05-13T23:24:22Z</dc:date>
    </item>
    <item>
      <title>Re: OpenCL1.2 Full Profile on QuadPlus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/OpenCL1-2-Full-Profile-on-QuadPlus/m-p/748292#M116368</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;what bsp version do you use? 4.9.11? how did you enable gpu? pls refer to enable it in the menuconfig as below:&lt;/P&gt;&lt;P&gt;CONFIG_MXC_GPU_VIV is a configuration option for GPU driver. In the menuconfig&lt;BR /&gt;this option is available under Device Drivers &amp;gt; MXC support drivers &amp;gt; MXC Vivante&lt;BR /&gt;GPU support &amp;gt; MXC Vivante GPU support.&lt;BR /&gt;On the screen displayed, select Configure the kernel, select Device Drivers &amp;gt; MXC&lt;BR /&gt;support drivers &amp;gt; MXC Vivante GPU support &amp;gt; MXC Vivante GPU support, and then&lt;BR /&gt;exit. When the next screen appears, select the following options to enable the GPU&lt;BR /&gt;driver:&lt;BR /&gt;• Package list &amp;gt; imx-gpu-viv&lt;BR /&gt;• This package provides proprietary binary libraries, and test code built from the GPU&lt;BR /&gt;for framebuffer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 May 2018 07:00:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/OpenCL1-2-Full-Profile-on-QuadPlus/m-p/748292#M116368</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-05-14T07:00:31Z</dc:date>
    </item>
    <item>
      <title>Re: OpenCL1.2 Full Profile on QuadPlus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/OpenCL1-2-Full-Profile-on-QuadPlus/m-p/748293#M116369</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Joan,&lt;/P&gt;&lt;P&gt;Yes, 4.9.11, both are configured (kernel config and imx-gpu-viv&amp;nbsp;package), the gpu is detected and works ok, driver is 6.2.2.p0, but on the QuadPlus the GPU is detected as 1.1 EP using Vivantes’s clinfo unit test&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 May 2018 15:21:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/OpenCL1-2-Full-Profile-on-QuadPlus/m-p/748293#M116369</guid>
      <dc:creator>tequilaguur</dc:creator>
      <dc:date>2018-05-14T15:21:33Z</dc:date>
    </item>
    <item>
      <title>Re: OpenCL1.2 Full Profile on QuadPlus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/OpenCL1-2-Full-Profile-on-QuadPlus/m-p/748294#M116370</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I double confirmed with GPU team, for imx6qp, which can support opencl 1.2 on HW, but on SW, still has some bugs, so now, SW supports opencl 1.1 only,&amp;nbsp; but imx6qp SW will support 1.2 later.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 May 2018 07:32:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/OpenCL1-2-Full-Profile-on-QuadPlus/m-p/748294#M116370</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2018-05-22T07:32:32Z</dc:date>
    </item>
    <item>
      <title>Re: OpenCL1.2 Full Profile on QuadPlus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/OpenCL1-2-Full-Profile-on-QuadPlus/m-p/748295#M116371</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Joan,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any tentative date that you can share with us to have OpenCL 1.2 Driver on imx6qp?@Joan Xie.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jun 2018 15:28:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/OpenCL1-2-Full-Profile-on-QuadPlus/m-p/748295#M116371</guid>
      <dc:creator>computerscience</dc:creator>
      <dc:date>2018-06-28T15:28:35Z</dc:date>
    </item>
  </channel>
</rss>