<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX7D SAI interface - rx delay</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-SAI-interface-rx-delay/m-p/747588#M116251</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using IMX7D SAI interface in master, synchronous mode.&lt;/P&gt;&lt;P&gt;It is configured to send /receive MSB first.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The slave device is able to receive the data, TX from SAI, properly.&lt;/P&gt;&lt;P&gt;But while sending, it is having a delay of 2 clock cycles.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a way to delay the RX word sampling start, by 2 clock cycles (from start of frame), in SAI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Aswin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 14 May 2018 06:59:48 GMT</pubDate>
    <dc:creator>aswinmohan</dc:creator>
    <dc:date>2018-05-14T06:59:48Z</dc:date>
    <item>
      <title>IMX7D SAI interface - rx delay</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-SAI-interface-rx-delay/m-p/747588#M116251</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using IMX7D SAI interface in master, synchronous mode.&lt;/P&gt;&lt;P&gt;It is configured to send /receive MSB first.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The slave device is able to receive the data, TX from SAI, properly.&lt;/P&gt;&lt;P&gt;But while sending, it is having a delay of 2 clock cycles.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a way to delay the RX word sampling start, by 2 clock cycles (from start of frame), in SAI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Aswin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 May 2018 06:59:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7D-SAI-interface-rx-delay/m-p/747588#M116251</guid>
      <dc:creator>aswinmohan</dc:creator>
      <dc:date>2018-05-14T06:59:48Z</dc:date>
    </item>
    <item>
      <title>Re: IMX7D SAI interface - rx delay</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-SAI-interface-rx-delay/m-p/747589#M116252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Aswin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it is possible to delay the RX word sampling by one clock using bit&lt;/P&gt;&lt;P&gt;FSE register I2Sx_RCR, but seems there is no option to delay for two clocks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 May 2018 18:56:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7D-SAI-interface-rx-delay/m-p/747589#M116252</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-05-14T18:56:45Z</dc:date>
    </item>
    <item>
      <title>Re: IMX7D SAI interface - rx delay</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX7D-SAI-interface-rx-delay/m-p/747590#M116253</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 May 2018 08:33:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX7D-SAI-interface-rx-delay/m-p/747590#M116253</guid>
      <dc:creator>aswinmohan</dc:creator>
      <dc:date>2018-05-15T08:33:46Z</dc:date>
    </item>
  </channel>
</rss>