<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Using MfgTool after Enabling Secure Feature (Locked Device)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-MfgTool-after-Enabling-Secure-Feature-Locked-Device/m-p/747556#M116248</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Sorry, but the information you are requesting is treated as confidential info at this time and requires a signed NDA (Non-Disclosure Agreement). Naturally, we cannot discuss this with you in public anyway, this requires to be handled as a Service Request (SR). Be aware that to give you remote support through a SR, we will still need the confirmation of a NXP employee that the NDA is in place.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Apr 2018 05:39:16 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2018-04-03T05:39:16Z</dc:date>
    <item>
      <title>Using MfgTool after Enabling Secure Feature (Locked Device)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-MfgTool-after-Enabling-Secure-Feature-Locked-Device/m-p/747555#M116247</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've successfully signed my u-boot and kernel, and enable the security fuse on the board. When integrating the signed images into my build I am able to use the software update perfectly fine. However, when using the MfgTool (manufacturing tool), I am unable to get it to flash the device.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to know it I should be able to use the MfgTool after I have locked the device, or if I should not be able to use the MfgTool after the secure fuse is enabled. Are there extra steps that I need to take to have the MfgTool working after i have enables the secure fuse?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, I am using MfgTool2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Mar 2018 14:53:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-MfgTool-after-Enabling-Secure-Feature-Locked-Device/m-p/747555#M116247</guid>
      <dc:creator>huzaifi</dc:creator>
      <dc:date>2018-03-28T14:53:26Z</dc:date>
    </item>
    <item>
      <title>Re: Using MfgTool after Enabling Secure Feature (Locked Device)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-MfgTool-after-Enabling-Secure-Feature-Locked-Device/m-p/747556#M116248</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Sorry, but the information you are requesting is treated as confidential info at this time and requires a signed NDA (Non-Disclosure Agreement). Naturally, we cannot discuss this with you in public anyway, this requires to be handled as a Service Request (SR). Be aware that to give you remote support through a SR, we will still need the confirmation of a NXP employee that the NDA is in place.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Apr 2018 05:39:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-MfgTool-after-Enabling-Secure-Feature-Locked-Device/m-p/747556#M116248</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2018-04-03T05:39:16Z</dc:date>
    </item>
  </channel>
</rss>