<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: About the VSNVS output voltage of PMIC and VDD_SNVS_IN input voltage of i.MX6 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/About-the-VSNVS-output-voltage-of-PMIC-and-VDD-SNVS-IN-input/m-p/746072#M116066</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; The selected in red variant of output PMIC SNVS voltage does not contradict&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;i.MX6 specs. Also, customers can use the case, based on external coin cell for &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;the PMIC: 2.84 V &amp;lt; VCOIN &amp;lt; 3.3 V.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Have a great day,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Yuri&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Note: If this post answers your question, please click the Correct Answer &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;button. Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Apr 2018 08:02:07 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2018-04-19T08:02:07Z</dc:date>
    <item>
      <title>About the VSNVS output voltage of PMIC and VDD_SNVS_IN input voltage of i.MX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-the-VSNVS-output-voltage-of-PMIC-and-VDD-SNVS-IN-input/m-p/746071#M116065</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We use i.MX6Solo and PF0100F0AEP.&lt;BR /&gt;I seem that a spec of the VSNVS output of PMIC do not match a spec of VDD_SNVS_IN.&lt;BR /&gt;I think that the Min value of VSNVS is less than the Min value of VDD_SNVS_IN.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does this affect the operation of i.MX6solo?&lt;BR /&gt;Or, Is it the mistake of specifications of which?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;For VDD_SNVS_IN of i.MX6Solo,&lt;BR /&gt;According to the "Table 8 Operating Ranges" in Datasheet, it is defined at 2.9V - 3.3V.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Table 8 Operating Ranges.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21386i66F4BEF20EC6C017/image-size/large?v=v2&amp;amp;px=999" role="button" title="Table 8 Operating Ranges.png" alt="Table 8 Operating Ranges.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, for VSNVS of PF0100,&lt;BR /&gt;According to the "Table 111. VSNVS electrical characteristics" in Datasheet, it is defined in 3.0V +/-5.0%.&lt;BR /&gt;So, the voltage range is from 2.85V to 3.15V.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Table 111. VSNVS electrical characteristics.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21596i339ECDB70217B84D/image-size/large?v=v2&amp;amp;px=999" role="button" title="Table 111. VSNVS electrical characteristics.png" alt="Table 111. VSNVS electrical characteristics.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;May I have an advice?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Yuuki&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Apr 2018 01:44:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-the-VSNVS-output-voltage-of-PMIC-and-VDD-SNVS-IN-input/m-p/746071#M116065</guid>
      <dc:creator>yuuki</dc:creator>
      <dc:date>2018-04-19T01:44:06Z</dc:date>
    </item>
    <item>
      <title>Re: About the VSNVS output voltage of PMIC and VDD_SNVS_IN input voltage of i.MX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-the-VSNVS-output-voltage-of-PMIC-and-VDD-SNVS-IN-input/m-p/746072#M116066</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp; The selected in red variant of output PMIC SNVS voltage does not contradict&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;i.MX6 specs. Also, customers can use the case, based on external coin cell for &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;the PMIC: 2.84 V &amp;lt; VCOIN &amp;lt; 3.3 V.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Have a great day,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Yuri&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Note: If this post answers your question, please click the Correct Answer &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;button. Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Apr 2018 08:02:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-the-VSNVS-output-voltage-of-PMIC-and-VDD-SNVS-IN-input/m-p/746072#M116066</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2018-04-19T08:02:07Z</dc:date>
    </item>
  </channel>
</rss>