<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: MIMXRT1050-EVK Drag And Drop FW Programming</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1050-EVK-Drag-And-Drop-FW-Programming/m-p/745658#M116029</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mark, thanks for the reply.&amp;nbsp; I have been using the IDE to program and debug applications in HyperFlash.&amp;nbsp; I am wondering why drag and drop specifically doesn't work.&amp;nbsp; This is an new processor and EVK and I was wondering if this was a bug or expected behavior, something I'm doing wrong etc.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 01 Dec 2017 15:39:13 GMT</pubDate>
    <dc:creator>ryanshuttlewort</dc:creator>
    <dc:date>2017-12-01T15:39:13Z</dc:date>
    <item>
      <title>MIMXRT1050-EVK Drag And Drop FW Programming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1050-EVK-Drag-And-Drop-FW-Programming/m-p/745655#M116026</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello I am using MCUXpresso IDE, version v10.1.0 [Build 589] [2017-11-14] with an MIMXRT1050-EVK SDK, version&amp;nbsp; &lt;SPAN class=""&gt;2.3.0&lt;/SPAN&gt; (2017-11-16).&amp;nbsp; I have been experimenting with the hello_world_xip example an have noticed that the drag and drop FW programming does not appear to be working. Any attempt to drag and drop the hello_world_xip build artifact (i.e. any .bin, .afx, .s19 etc.) results in a long pause, followed by a reset and the appearance of a file named FAIL.TXT which contains the text "The transfer timed out."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the proper procedure?&lt;/P&gt;&lt;P&gt;What file types are supported?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Nov 2017 17:26:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1050-EVK-Drag-And-Drop-FW-Programming/m-p/745655#M116026</guid>
      <dc:creator>ryanshuttlewort</dc:creator>
      <dc:date>2017-11-29T17:26:41Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1050-EVK Drag And Drop FW Programming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1050-EVK-Drag-And-Drop-FW-Programming/m-p/745656#M116027</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ryan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please take a look to the attached document. If the problem persists please consider what suggested here &lt;A href="https://community.nxp.com/thread/464927"&gt;MCUXpresso and RT1050 HyperFlash Programming&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Dec 2017 00:31:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1050-EVK-Drag-And-Drop-FW-Programming/m-p/745656#M116027</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2017-12-01T00:31:48Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1050-EVK Drag And Drop FW Programming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1050-EVK-Drag-And-Drop-FW-Programming/m-p/745657#M116028</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ryan,&lt;/P&gt;&lt;P&gt;You are specifically using MCUX 10.1 and the interface with hyperflash is somewhat more straightforward, compared to IAR.&amp;nbsp;&lt;/P&gt;&lt;P&gt;MCUX is using a flash driver loaded through the debugger to program the hyperflash, and you do not need to put the EVK into SDP mode with SW7 to load the image to flash.&lt;/P&gt;&lt;P&gt;Here is the procedure:&lt;/P&gt;&lt;P&gt;1) Make certain that you have a USB connection via J28, that the power jumper J1 has header 5:6, and your board is enumerated correctly by the host interface - you should see the drive EVK-MIMXRT.&lt;/P&gt;&lt;P&gt;2) Confirm the version of&amp;nbsp;DAPLink firmware on the debugger -&amp;gt; open the file DETAILS.TXT on the EVK-MIMXRT drive and confirm that 'Interface Version' is at least 0244.&lt;/P&gt;&lt;P&gt;3) Leave boot mode switches on J7 as 0-1-1-0 : you will not need to move these at any point.&lt;/P&gt;&lt;P&gt;4) Compile the hello_world_xip code, you'll get an output file evkmimxrt1050_demo_apps_hello_world_xip.axf.&lt;/P&gt;&lt;P&gt;5) Run a debug session (use the Quickstart Panel) &amp;amp; MCUX automatically flashes the image... it should not take more that 5 seconds, and the image is executed up to the c-language entry point main(). Then of course you'll get debug control.&lt;/P&gt;&lt;P&gt;6) If you don't want to use the semi-hosting interface, you can easy modify the SDK Debug Console output to UART (I mean, VCOM via the DAPLink) with the Quick Settings&amp;gt;&amp;gt; menu in the QuickStart Panel. Obviously you will need to stop the debugger, rebuild &amp;amp; flash your code, and use TeraTerm, PuTTY or equivalent.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Happy flashing. Let us know how you get on.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Dec 2017 15:11:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1050-EVK-Drag-And-Drop-FW-Programming/m-p/745657#M116028</guid>
      <dc:creator>UK_CF_FAE</dc:creator>
      <dc:date>2017-12-01T15:11:42Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1050-EVK Drag And Drop FW Programming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1050-EVK-Drag-And-Drop-FW-Programming/m-p/745658#M116029</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mark, thanks for the reply.&amp;nbsp; I have been using the IDE to program and debug applications in HyperFlash.&amp;nbsp; I am wondering why drag and drop specifically doesn't work.&amp;nbsp; This is an new processor and EVK and I was wondering if this was a bug or expected behavior, something I'm doing wrong etc.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Dec 2017 15:39:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1050-EVK-Drag-And-Drop-FW-Programming/m-p/745658#M116029</guid>
      <dc:creator>ryanshuttlewort</dc:creator>
      <dc:date>2017-12-01T15:39:13Z</dc:date>
    </item>
  </channel>
</rss>