<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx6ULL EVK flash memory settings</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6ULL-EVK-flash-memory-settings/m-p/744323#M115848</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Stefano&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for using NAND with i.MX6ULL EVK one can follow i.MX 6ULL EVK Board Hardware User's Guide,&lt;/P&gt;&lt;P&gt;remove the QSPI Nor flash device.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/user-guide/IMX6ULLEVKHUG.pdf" title="https://www.nxp.com/docs/en/user-guide/IMX6ULLEVKHUG.pdf"&gt;https://www.nxp.com/docs/en/user-guide/IMX6ULLEVKHUG.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;One can try to boot from SD1 and test NAND interface, checking signals with oscilloscope&lt;/P&gt;&lt;P&gt;(BOOT_CFG are not used in that case).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Apr 2018 23:37:17 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2018-04-18T23:37:17Z</dc:date>
    <item>
      <title>imx6ULL EVK flash memory settings</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ULL-EVK-flash-memory-settings/m-p/744322#M115847</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear community, I solder a NAND flash module on the imx6ull EVK.&lt;/P&gt;&lt;P&gt;The flash module is the MT29F4G08ABADAWP (the 4Gb IT) from MICRON, I attach the data sheet.&lt;/P&gt;&lt;P&gt;After solder the module we use the mfgtools2, but unfortunately I am unable to see the module and there is no way to interact with it. Of course I try with the u-boot with NAND support, but the NAND field report 0MB and no one operation like "nand info" are working on my side.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found a document that explain how to setup some resistors on CU module to enable the NAND flash, you can see this document at page 9 of the attached pdf file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My thoughts are to set the BOOT_CFG1 in this way:&lt;/P&gt;&lt;P&gt;bit set &lt;BR /&gt; 0 1 &lt;BR /&gt; 1 0 &lt;BR /&gt; 2 0 &lt;BR /&gt; 3 0 &lt;BR /&gt; 4 1 &lt;BR /&gt; 5 0 &lt;BR /&gt; 6 0 &lt;BR /&gt; 7 1 &lt;BR /&gt; and to set BOOT_CFG2 in this way: &lt;BR /&gt; bit set &lt;BR /&gt; 0 0 &lt;BR /&gt; 1 0 &lt;BR /&gt; 2 0 &lt;BR /&gt; 3 0 &lt;BR /&gt; 4 0 &lt;BR /&gt; 5 0 &lt;BR /&gt; 6 0 &lt;BR /&gt; 7 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have no concern about BOOT_CFG4, because I don't clearly understand how it works and how it could help to setup the NAND communication.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone confirm my setup for BOOT_CFG1, BOOT_CFG2 and BOOT_CFG4?&lt;/P&gt;&lt;P&gt;Is this the reason that I am unable to see the NAND flash from u-boot?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help will be appreciated,&lt;/P&gt;&lt;P&gt;Stefano.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Apr 2018 10:01:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ULL-EVK-flash-memory-settings/m-p/744322#M115847</guid>
      <dc:creator>SCordibella</dc:creator>
      <dc:date>2018-04-18T10:01:11Z</dc:date>
    </item>
    <item>
      <title>Re: imx6ULL EVK flash memory settings</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ULL-EVK-flash-memory-settings/m-p/744323#M115848</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Stefano&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for using NAND with i.MX6ULL EVK one can follow i.MX 6ULL EVK Board Hardware User's Guide,&lt;/P&gt;&lt;P&gt;remove the QSPI Nor flash device.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/user-guide/IMX6ULLEVKHUG.pdf" title="https://www.nxp.com/docs/en/user-guide/IMX6ULLEVKHUG.pdf"&gt;https://www.nxp.com/docs/en/user-guide/IMX6ULLEVKHUG.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;One can try to boot from SD1 and test NAND interface, checking signals with oscilloscope&lt;/P&gt;&lt;P&gt;(BOOT_CFG are not used in that case).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Apr 2018 23:37:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ULL-EVK-flash-memory-settings/m-p/744323#M115848</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-04-18T23:37:17Z</dc:date>
    </item>
    <item>
      <title>Re: imx6ULL EVK flash memory settings</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ULL-EVK-flash-memory-settings/m-p/744324#M115849</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor, yes, we remove the NOR flash and we follow the instructions. Now we are able to boot from SD card, but I don't understand what you mean when you say checking signal with oscilloscope. Can you give me an example?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your time,&lt;/P&gt;&lt;P&gt;Stefano.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Apr 2018 06:18:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ULL-EVK-flash-memory-settings/m-p/744324#M115849</guid>
      <dc:creator>SCordibella</dc:creator>
      <dc:date>2018-04-19T06:18:30Z</dc:date>
    </item>
    <item>
      <title>Re: imx6ULL EVK flash memory settings</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ULL-EVK-flash-memory-settings/m-p/744325#M115850</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Stefano&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check #ifdef CONFIG_SYS_USE_NAND&amp;nbsp; in uboot/include/configs/mx6ullevk.h :&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/include/configs/mx6ullevk.h?h=imx_v2016.03_4.1.15_2.0.0_ga&amp;amp;id=rel_imx_4.1.15_2.1.0_ga" title="http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/include/configs/mx6ullevk.h?h=imx_v2016.03_4.1.15_2.0.0_ga&amp;amp;id=rel_imx_4.1.15_2.1.0_ga"&gt;uboot-imx.git - Freescale i.MX u-boot Tree&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;if you unable to see the NAND flash from u-boot then there may be errors&lt;/P&gt;&lt;P&gt;in connection and one can start to debug it with oscilloscope.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Apr 2018 09:45:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ULL-EVK-flash-memory-settings/m-p/744325#M115850</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-04-19T09:45:40Z</dc:date>
    </item>
  </channel>
</rss>