<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックQuad NXP i.MX6 ARM CPU Core Power Dissipation</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Quad-NXP-i-MX6-ARM-CPU-Core-Power-Dissipation/m-p/742599#M115585</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;I need &lt;SPAN style="color: red;"&gt;Power Dissipation &lt;/SPAN&gt;information of this Quad Processor &amp;nbsp;we are running this at full capacity. WE are selecting a other Heat sink , for that we need power dissipation&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;So if anyone&amp;nbsp;can tell &amp;nbsp;the power dissipation in Quad Core so we can select other heat sink.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Mar 2018 06:50:35 GMT</pubDate>
    <dc:creator>kunalbarot</dc:creator>
    <dc:date>2018-03-09T06:50:35Z</dc:date>
    <item>
      <title>Quad NXP i.MX6 ARM CPU Core Power Dissipation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Quad-NXP-i-MX6-ARM-CPU-Core-Power-Dissipation/m-p/742599#M115585</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;I need &lt;SPAN style="color: red;"&gt;Power Dissipation &lt;/SPAN&gt;information of this Quad Processor &amp;nbsp;we are running this at full capacity. WE are selecting a other Heat sink , for that we need power dissipation&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;So if anyone&amp;nbsp;can tell &amp;nbsp;the power dissipation in Quad Core so we can select other heat sink.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Mar 2018 06:50:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Quad-NXP-i-MX6-ARM-CPU-Core-Power-Dissipation/m-p/742599#M115585</guid>
      <dc:creator>kunalbarot</dc:creator>
      <dc:date>2018-03-09T06:50:35Z</dc:date>
    </item>
    <item>
      <title>Re: Quad NXP i.MX6 ARM CPU Core Power Dissipation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Quad-NXP-i-MX6-ARM-CPU-Core-Power-Dissipation/m-p/742600#M115586</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kunal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please look on AN4509 i.MX6Dual/6Quad Power Consumption Measurement&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://cache.freescale.com/files/32bit/doc/app_note/AN4509.pdf" title="https://cache.freescale.com/files/32bit/doc/app_note/AN4509.pdf"&gt;https://cache.freescale.com/files/32bit/doc/app_note/AN4509.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and AN4579 i.MX 6 Series Thermal Management Guidelines&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://cache.freescale.com/files/32bit/doc/app_note/AN4579.pdf" title="https://cache.freescale.com/files/32bit/doc/app_note/AN4579.pdf"&gt;https://cache.freescale.com/files/32bit/doc/app_note/AN4579.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Mar 2018 07:49:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Quad-NXP-i-MX6-ARM-CPU-Core-Power-Dissipation/m-p/742600#M115586</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2018-03-09T07:49:58Z</dc:date>
    </item>
    <item>
      <title>Re: Quad NXP i.MX6 ARM CPU Core Power Dissipation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Quad-NXP-i-MX6-ARM-CPU-Core-Power-Dissipation/m-p/742601#M115587</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kunal,&lt;/P&gt;&lt;P&gt;The two documents that Igor pointed will help. But each board is different - what you need to do is measure the power consumption of your own board in worst case scenario.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are two main power rails going into the processor one is core voltage ( typically at 1.34V) and other is DDR voltage ( typically at 1.5V). Add like a 0.02 Ohm resistor in series and then run your software. Measure current and note down power consumption.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While you are doing it, measure the CPU temperature ( you can write a shell script to record temperature at like every 3 seconds).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once you have done this exercise, you will have an idea where you stand. Then add heatsink and repeat the exercise.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Mar 2018 08:13:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Quad-NXP-i-MX6-ARM-CPU-Core-Power-Dissipation/m-p/742601#M115587</guid>
      <dc:creator>lokesh</dc:creator>
      <dc:date>2018-03-09T08:13:02Z</dc:date>
    </item>
    <item>
      <title>Re: Quad NXP i.MX6 ARM CPU Core Power Dissipation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Quad-NXP-i-MX6-ARM-CPU-Core-Power-Dissipation/m-p/742602#M115588</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Vikas&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the Reponse, I have already done this , I measure the Power consumption comes approx 8-10W. (when most of peripheral working). &amp;nbsp;But What I am looking for is Power dissipation , I believe its different than the power consumption , it is the power which lost in Heat. So i need that figure so I can calculate and select proper Heat Sink.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Mar 2018 08:54:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Quad-NXP-i-MX6-ARM-CPU-Core-Power-Dissipation/m-p/742602#M115588</guid>
      <dc:creator>kunalbarot</dc:creator>
      <dc:date>2018-03-09T08:54:28Z</dc:date>
    </item>
    <item>
      <title>Re: Quad NXP i.MX6 ARM CPU Core Power Dissipation</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Quad-NXP-i-MX6-ARM-CPU-Core-Power-Dissipation/m-p/742603#M115589</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;All power that is consumed by your board eventually gets converted into heat, of course, minus any light energy that will typically be dissipating through, say, backlight in an LCD. Or I am missing something here.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The 8-10 W is a close to what I measured as well. Did you also measure the die temperature under peak load ? How much it was ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can use the following command, for example to see CPU die temperature&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;cat /sys/class/thermal/thermal_zone0/temp&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From here the problem goes into thermal simulation domain - to get precise answer of&amp;nbsp; the Heat Sink Size etc. We can get quick answer by using some off the shelf heatsink ( there are many available at digikey to fit in for i.MX6) and see if it makes the i.MX6 die temperature acceptable.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Mar 2018 15:43:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Quad-NXP-i-MX6-ARM-CPU-Core-Power-Dissipation/m-p/742603#M115589</guid>
      <dc:creator>lokesh</dc:creator>
      <dc:date>2018-03-09T15:43:24Z</dc:date>
    </item>
  </channel>
</rss>