<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: [Android 4.4.3] How to setting or modify for mount USB storage in host USB port?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Android-4-4-3-How-to-setting-or-modify-for-mount-USB-storage-in/m-p/742188#M115530</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Victor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; On our i.MX6QDL SabreSD board, only USB OTG is supported. And the USB OTG is desgined to be dual role mode. so if you want to test it's Host mode, you should connect a USB OTG to HOST cable to MicroUSB connector, and connect USB device on the other side.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; If you are using the Evaluation board, you don't need to modify android source code. the function has been supported.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[Note] For USB OTG , there 2 kinds of cable:&lt;/P&gt;&lt;P&gt;-----USB OTG cable : it makes USB OTG work at device mode, such as USB charging cable for mobile.&lt;/P&gt;&lt;P&gt;-----USB OTG to Host cable: when the cable is connected to microUSB connector, USB_OTG_ID can be pulled down to LOW, and USB OTG working at HOST mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;P&gt;TIC weidong sun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 04 Jun 2018 02:25:34 GMT</pubDate>
    <dc:creator>weidong_sun</dc:creator>
    <dc:date>2018-06-04T02:25:34Z</dc:date>
    <item>
      <title>[Android 4.4.3] How to setting or modify for mount USB storage in host USB port?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-4-4-3-How-to-setting-or-modify-for-mount-USB-storage-in/m-p/742187#M115529</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I'm using i.MX6 sabreSD DL.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In device/fsl/&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;sabresd_6dq/fstab.freescale, I modify the file below.&lt;/SPAN&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;/devices/soc0/soc.1/2100000.aips-bus/2198000.usdhc/mmc_host /mnt/media_rw/extsd vfat defaults voldmanaged=extsd:auto&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;/devices/soc0/soc.1/2100000.aips-bus/2184000.usb/ci_hdrc.0 /mnt/media_rw/udisk vfat defaults voldmanaged=udisk:auto&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;/devices/soc0/soc.1/2100000.aips-bus/2184200.usb/ci_hdrc.1* /mnt/media_rw/udisk vfat defaults voldmanaged=udisk:auto&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/dev/block/mmcblk3p5 /system ext4 ro wait&lt;BR /&gt;/dev/block/mmcblk3p4 /data ext4 nosuid,nodev,nodiratime,noatime,nomblk_io_submit,noauto_da_alloc,errors=panic wait,encryptable=footer&lt;BR /&gt;/dev/block/mmcblk3p6 /cache ext4 nosuid,nodev,nomblk_io_submit wait&lt;BR /&gt;/dev/block/mmcblk3p7 /device ext4 ro,nosuid,nodev wait&lt;BR /&gt;/dev/block/mmcblk3p1 /boot emmc defaults defaults&lt;BR /&gt;/dev/block/mmcblk3p2 /recovery emmc defaults defaults&lt;BR /&gt;/dev/block/mmcblk3p8 /misc emmc defaults defaults&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I cannot see my storage under /storage in system.&lt;/P&gt;&lt;P&gt;Did I miss anything here?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Jun 2018 05:58:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-4-4-3-How-to-setting-or-modify-for-mount-USB-storage-in/m-p/742187#M115529</guid>
      <dc:creator>wangvictor</dc:creator>
      <dc:date>2018-06-01T05:58:14Z</dc:date>
    </item>
    <item>
      <title>Re: [Android 4.4.3] How to setting or modify for mount USB storage in host USB port?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-4-4-3-How-to-setting-or-modify-for-mount-USB-storage-in/m-p/742188#M115530</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Victor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; On our i.MX6QDL SabreSD board, only USB OTG is supported. And the USB OTG is desgined to be dual role mode. so if you want to test it's Host mode, you should connect a USB OTG to HOST cable to MicroUSB connector, and connect USB device on the other side.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; If you are using the Evaluation board, you don't need to modify android source code. the function has been supported.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[Note] For USB OTG , there 2 kinds of cable:&lt;/P&gt;&lt;P&gt;-----USB OTG cable : it makes USB OTG work at device mode, such as USB charging cable for mobile.&lt;/P&gt;&lt;P&gt;-----USB OTG to Host cable: when the cable is connected to microUSB connector, USB_OTG_ID can be pulled down to LOW, and USB OTG working at HOST mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;P&gt;TIC weidong sun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Jun 2018 02:25:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-4-4-3-How-to-setting-or-modify-for-mount-USB-storage-in/m-p/742188#M115530</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2018-06-04T02:25:34Z</dc:date>
    </item>
    <item>
      <title>Re: [Android 4.4.3] How to setting or modify for mount USB storage in host USB port?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-4-4-3-How-to-setting-or-modify-for-mount-USB-storage-in/m-p/742189#M115531</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What I mean is to plug my USB storage in i.MX6DL SabreSD board.&lt;/P&gt;&lt;P&gt;And system do recognize that usb device&amp;nbsp;is plug in.&lt;/P&gt;&lt;P&gt;But the system did not mount it under /storage .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can not understand is there any relative&amp;nbsp;to USB OTG ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Jun 2018 03:49:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-4-4-3-How-to-setting-or-modify-for-mount-USB-storage-in/m-p/742189#M115531</guid>
      <dc:creator>wangvictor</dc:creator>
      <dc:date>2018-06-04T03:49:55Z</dc:date>
    </item>
  </channel>
</rss>